asm/linkage.h missing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

asm/linkage.h missing

ソリューションへジャンプ
10,401件の閲覧回数
amin_rahimi
Contributor II

I'm trying to use libvpu and libipu to display H264 video streams on my Nitrogen6x.  I had no issues with this in Dora, but when I updated to Dizzy, I came across a new error that I haven't been able to resolve when using linux/mxcfb.h.  The g++ command line and error are:

cd /home/rahimia/dizzy/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/mocu3/1.0-r0/build/MediaModules/VPUCodec && /home/rahimia/dizzy/build/tmp/sysroots/x86_64-linux/usr/bin/arm-poky-linux-gnueabi/arm-poky-linux-gnueabi-g++   -DBOOST_ALL_NO_LIB -DBUILD_FOR_ARM -DVPUCodec_EXPORTS -march=armv7-a -mthumb-interwork -mfloat-abi=hard -mfpu=neon -mtune=cortex-a9  --sysroot=/home/rahimia/dizzy/build/tmp/sysroots/nitrogen6x  -O2 -pipe -g -feliminate-unused-debug-types -fvisibility-inlines-hidden -std=c++0x -fpermissive -fPIC -g -I/home/rahimia/dizzy/build/tmp/sysroots/nitrogen6x/usr/include -I/home/rahimia/dizzy/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/mocu3/1.0-r0/trunk/Common/include -I/home/rahimia/dizzy/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/mocu3/1.0-r0/trunk/Common/lib -I/home/rahimia/dizzy/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/mocu3/1.0-r0/trunk/MediaModules/VPUCodec/. -I/home/rahimia/dizzy/build/tmp/sysroots/nitrogen6x/usr/src/kernel/include    -o CMakeFiles/VPUCodec.dir/dllmain.cpp.o -c /home/rahimia/dizzy/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/mocu3/1.0-r0/trunk/MediaModules/VPUCodec/dllmain.cpp

In file included from /home/rahimia/dizzy/build/tmp/sysroots/nitrogen6x/usr/src/kernel/include/linux/kgdb.h:16:0,

                 from /home/rahimia/dizzy/build/tmp/sysroots/nitrogen6x/usr/src/kernel/include/linux/fb.h:4,

                 from /home/rahimia/dizzy/build/tmp/sysroots/nitrogen6x/usr/src/kernel/include/uapi/linux/mxcfb.h:31,

                 from /home/rahimia/dizzy/build/tmp/sysroots/nitrogen6x/usr/src/kernel/include/linux/mxcfb.h:24,

                 from /home/rahimia/dizzy/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/mocu3/1.0-r0/trunk/MediaModules/VPUCodec/IPUDisplay.h:27,

                 from /home/rahimia/dizzy/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/mocu3/1.0-r0/trunk/MediaModules/VPUCodec/Decoder.h:14,

                 from /home/rahimia/dizzy/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/mocu3/1.0-r0/trunk/MediaModules/VPUCodec/VPUCodec.h:6,

                 from /home/rahimia/dizzy/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/mocu3/1.0-r0/trunk/MediaModules/VPUCodec/dllmain.cpp:3:

/home/rahimia/dizzy/build/tmp/sysroots/nitrogen6x/usr/src/kernel/include/linux/linkage.h:7:25: fatal error: asm/linkage.h: No such file or directory

#include <asm/linkage.h>

I've tried adding include paths and symbolic links to the directories I thought I needed, but ultimately couldn't resolve the issue.  I did notice that there's no longer a "plat-mxc" directory under the kernel source.  Is this an issue?

I have PREFERRED_PROVIDER_virtual/kernel = "linux-boundary"  and PREFERRED_VERSION_linux-boundary = "3.10.17" in my local.conf and I'm building the image with imx-lib and imx-vpu.

ラベル(3)
0 件の賞賛
返信
1 解決策
5,216件の閲覧回数
amin_rahimi
Contributor II

Fixed.  I needed .../usr/src/kernel/include/uapi to be included before .../usr/src/kernel/include.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
5,217件の閲覧回数
amin_rahimi
Contributor II

Fixed.  I needed .../usr/src/kernel/include/uapi to be included before .../usr/src/kernel/include.

0 件の賞賛
返信