armnn build error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

armnn build error

1,361 Views
Chayma
Contributor III

Hello everyone,

I have been struggling with an error while building an image for imx8m using yocto.
The error appeared in the armnn_do_compile step
ERROR: Logfile of failure stored in: tmp/work/aarch64-poky-linux/armnn/19.08-r1/temp/log.do_compile.22133
NOTE: recipe armnn-19.08-r1: task do_compile: Failed
ERROR: Task (sources/meta-imx/meta-ml/recipes-libraries/armnn/armnn_git.bb:do_compile) failed with exit code '1'

Note :
1- Ubuntu 20.04.2 LTS

2- NXP Release : imx-5.4.24-2.1.0

3- I rechecked all Yocto system requirement and dependencies

 

Thank you in advance.

0 Kudos
Reply
1 Reply

1,357 Views
nxf63675
NXP TechSupport
NXP TechSupport

Hi  @Chayma,

 

Please share the steps that you are doing to build your image, I will try to duplicate your issue from my site.

 

Regards,

Israel.

0 Kudos
Reply