arm hard float point

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

arm hard float point

2,900件の閲覧回数
allen_kim1
Contributor I

Dear Community 

i have a question about arm hard float point option 

we need arm float point option on LTIB tool chain 

i write some example code and compile with  LTIB , yocto 

binary that compiled with LTIB has no FLAGS (  hard-float ABI ) 

binary that compiled with yocto  has a  hard-float ABI FLAGS

LTIB latest toolchain ( 20130816 version ) 

/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-fsl-linux-gnueabi-gcc -c float_sum.cpp  -march=armv7-a -mfloat-abi=hard -mfpu=neon -mtune=cortex-a9

/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-fsl-linux-gnueabi-gcc  -o float_test float_sum.o float_test.cpp  -march=armv7-a -mfloat-abi=hard -mfpu=neon -mtune=cortex-a9 -lpthread

allen_kim@host:~/test_hf/src$ readelf  -h float_test

ELF Header:

  Magic:   7f 45 4c 46 01 01 01 00 00 00 00 00 00 00 00 00

  Class:                             ELF32

  Data:                              2's complement, little endian

  Version:                           1 (current)

  OS/ABI:                            UNIX - System V

  ABI Version:                       0

  Type:                              EXEC (Executable file)

  Machine:                           ARM

  Version:                           0x1

  Entry point address:               0x83c4

  Start of program headers:          52 (bytes into file)

  Start of section headers:          2396 (bytes into file)

  Flags:                             0x5000002, has entry point, Version5 EABI

  Size of this header:               52 (bytes)

  Size of program headers:           32 (bytes)

  Number of program headers:         8

  Size of section headers:           40 (bytes)

  Number of section headers:         30

  Section header string table index: 27

yocto 4.1.15 toolchain

/opt/fsl-imx-fb/4.1.15-1.1.1/sysroots/x86_64-pokysdk-linux/usr/bin/arm-poky-linux-gnueabi/arm-poky-linux-gnueabi-gcc -c float_sum.cpp -march=armv7-a -mfloat-abi=hard -mfpu=neon -mtune=cortex-a9 --sysroot=/opt/fsl-imx-fb/4.1.15-

1.1.1/sysroots/cortexa9hf-vfp-neon-poky-linux-gnueabi/
/opt/fsl-imx-fb/4.1.15-1.1.1/sysroots/x86_64-pokysdk-linux/usr/bin/arm-poky-linux-gnueabi/arm-poky-linux-gnueabi-gcc -o float_test_yocto float_sum.o float_test.cpp -march=armv7-a -mfloat-abi=hard -mfpu=neon -mtune=cortex-a9 -lpthread --sysroot=/opt/fsl-imx-fb/4.1.15-1.1.1/sysroots/cortexa9hf-vfp-neon-poky-linux-gnueabi/

allen_kim@host:~/test_hf/src$ readelf  -h float_test_yocto

ELF Header:

  Magic:   7f 45 4c 46 01 01 01 00 00 00 00 00 00 00 00 00

  Class:                             ELF32

  Data:                              2's complement, little endian

  Version:                           1 (current)

  OS/ABI:                            UNIX - System V

  ABI Version:                       0

  Type:                              EXEC (Executable file)

  Machine:                           ARM

  Version:                           0x1

  Entry point address:               0x10444

  Start of program headers:          52 (bytes into file)

  Start of section headers:          9228 (bytes into file)

  Flags:                             0x5000402, has entry point, Version5 EABI, hard-float ABI

  Size of this header:               52 (bytes)

  Size of program headers:           32 (bytes)

  Number of program headers:         8

  Size of section headers:           40 (bytes)

  Number of section headers:         39

  Section header string table index: 36

how can i support hard-float ABI in LTIB crosstool chain ?

please guide me 

Thanks BR

ラベル(3)
タグ(3)
0 件の賞賛
返信
1 返信

2,267件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello

  I hope the following helps.

https://community.nxp.com/message/862949 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 件の賞賛
返信