apt is not working in imx6qsabresd

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

apt is not working in imx6qsabresd

1,309 Views
lakshmikanthr
Contributor III

Hi,

apt is not working in imx6qsabresd. do u have any idea regrading this. I am looking forward for reply. 

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

1,234 Views
Carlos_Musich
NXP Employee
NXP Employee

If you are using Yocto you will find this useful: How do I - Yocto Project 


Best regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,234 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

Could you tell me which version BSP are you using?

Have a nice day

Rita

0 Kudos
Reply

1,234 Views
lakshmikanthr
Contributor III

Hi,

Thank you for acknowledging.

I am using yocto 2.2 Morty branch .I am looking forward for your reply.

Thanks & Regards,

R.lakshmikanth

0 Kudos
Reply