Is there a supported for the SABRE board with kernel 3.14.52 & Qt5.7 or greater?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a supported for the SABRE board with kernel 3.14.52 & Qt5.7 or greater?

2,401 Views
kengyulin
Contributor II

I have an i.MX6DL SABRE board, and I'm trying to get a modern build for it. I'm looking to find a Yocto release, 3.14.52 kernel, Qt5.7.1 or greater.

I attempted to sync/build this:

 

$ repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.14.52-1.1.0_ga

$ repo sync

$ MACHINE=imx6dlsabresd source fsl-setup-release.sh -b build_qt5 -e fb

$ bitbake -k fsl-image-qt5

But it seem that this package only contain Qt5.5

But if I change the /sources/meta-qt5 by command:

$ git clone -b master https://github.com/meta-qt5/meta-qt5.git

and then try again

$ MACHINE=imx6dlsabresd source fsl-setup-release.sh -b build_qt5 -e fb

$ bitbake -k fsl-image-qt5

It shows that:

ERROR: ParseError at /home/scout/freescale-3.14-try2/sources/meta-qt5/classes/qmake5_base.bbclass:48: Could not inherit file classes/remove-libtool.bbclass

and then stop

Can someone help me?

2017/08/04 update: 

If I edit ~/freescale-3.14-try2/sources/meta-qt5/classes/qmake5_base.bbclass file

Ln 50 : -- inherit qmake5_paths remove-libtool

            ++ inherit qmake5_paths

It can go through, but still stop at the other qt build task.

Now status : pending, and go through another way. (Try porting to kernel4.1.15 EX: https://community.nxp.com/docs/DOC-333580 )

Thanks everyone who answer to me, and if anyone still have some answer to share, I would be very grateful.

Labels (4)
Tags (3)
4 Replies

2,054 Views
joanxie
NXP TechSupport
NXP TechSupport

pls refer to the qt document, hope helpful for you

Building Your Own Embedded Linux Image | Qt 5.9.1 for Device Creation 

2,054 Views
kengyulin
Contributor II

Thanks for your response.
I've already done this part with Qt5.9 with 30days license. But the default kernel is 4.X, is there anyway change the Boot2Qt's Yocto to fit the kernel 3.14.

0 Kudos
Reply

2,054 Views
joanxie
NXP TechSupport
NXP TechSupport

yes, you should update your kernel, so you must use 3.14.52 kernel and qt 5.7??

0 Kudos
Reply

2,054 Views
kengyulin
Contributor II

Qt 5.6 is ok, because I need to use Qt can bus.

If I can't use 3.14.52 kernel, I need to porting to 4.X kernel myself. It's maybe a very big effort.

0 Kudos
Reply