android6.0 imx6q & imx6dl system reboot when u disk quick plug test

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

android6.0 imx6q & imx6dl system reboot when u disk quick plug test

3,701 次查看
昌清黄
Contributor I
There are two cases:


[ 21.511305] init: Service 'bootanim' (pid 305) exited with status 0
[ 21.806715] acc_open
[ 21.809151] acc_release
[ 29.740610] FAT-fs (sda1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[ 32.296394] init: write_file: Unable to open '/sys/devices/system/cpu/cpu0/cpufreq/scaling_governor': No such file or directory
[ 32.308722] init: write_file: Unable to open '/sys/devices/system/cpu/cpufreq/interactive/timer_rate': No such file or directory
[ 32.308797] init: write_file: Unable to open '/sys/devices/system/cpu/cpufreq/interactive/min_sample_time': No such file or directory
[ 32.308855] init: write_file: Unable to open '/sys/devices/system/cpu/cpufreq/interactive/go_hispeed_load': No such file or directory
[ 97.152276] usb 1-1.4: USB disconnect, device number 4
[ 97.352693] FAT-fs (sda1): Directory bread(block 14197536) failed
[ 97.359002] FAT-fs (sda1): Directory bread(block 14197537) failed
[ 97.365231] FAT-fs (sda1): Directory bread(block 14197538) failed
[ 97.371422] FAT-fs (sda1): Directory bread(block 14197539) failed
[ 97.377685] FAT-fs (sda1): Directory bread(block 14197540) failed
[ 97.383883] FAT-fs (sda1): Directory bread(block 14197541) failed
[ 97.390154] FAT-fs (sda1): Directory bread(block 14197542) failed
[ 97.396402] FAT-fs (sda1): Directory bread(block 14197543) failed
[ 97.402594] FAT-fs (sda1): Directory bread(block 14197544) failed
[ 97.408876] FAT-fs (sda1): Directory bread(block 14197545) failed
[ 107.954723] Unable to handle kernel paging request at virtual address 2de3e000
[ 107.961967] pgd = d2ae4000
[ 107.964680] [2de3e000] *pgd=00000000
[ 107.968285] Internal error: Oops: 5 [#1] PREEMPT SMP ARM
[ 107.973604] Modules linked in:
[ 107.976685] CPU: 0 PID: 228 Comm: vold Not tainted 4.1.15 #72
[ 107.982439] Hardware name: Freescale i.MX6 Quad/DualLite (Device Tree)
[ 107.988975] task: d2a6ce00 ti: d2c08000 task.ti: d2c08000
[ 107.994396] PC is at __percpu_counter_add+0x30/0x104
[ 107.999369] LR is at __percpu_counter_add+0x28/0x104
[ 108.004342] pc : [<c04e3984>] lr : [<c04e397c>] psr: 20010093
[ 108.004342] sp : d2c09de8 ip : 00000000 fp : 00000008
[ 108.015825] r10: d165eab0 r9 : d1554600 r8 : 00000000
[ 108.021055] r7 : 00000000 r6 : 00000001 r5 : 00000018 r4 : d27892e8
[ 108.027587] r3 : 00000000 r2 : 2de3e000 r1 : c0e46160 r0 : 00000000
[ 108.034121] Flags: nzCv IRQs off FIQs on Mode SVC_32 ISA ARM Segment user
[ 108.041350] Control: 10c53c7d Table: 22ae404a DAC: 00000015
[ 108.047101]
[ 108.047101] PC: 0xc04e3904:
[ 108.051377] 3904 e3e00000 ea000004 e79a2100 e5963018 e7933002 e0944003 e0a55fc3 e2802001
[ 108.059715] 3924 e3a01004 e1a00007 ebff4dbe e5993000 e1500003 bafffff3 e1a00006 e1a01008
[ 108.068044] 3944 eb1956e2 e1a00004 e1a01005 e8bd87f0 e92d43f8 e1a04000 e3a00001 e1a06002
[ 108.076381] 3964 e1a07003 e59d5020 ebf1cf0d e3060160 e34c00e4 ebffc495 e5943018 ee1d2f90
[ 108.084708] 3984 e7923003 e1a01fc5 e0968003 e0a79fc3 e1580005 e0d93001 aa000004 e2652000
[ 108.093045] 39a4 e1520008 e1a03fc2 e0d33009 ba00001f e1a00004 e0686006 eb19562b e1c420d8
[ 108.101373] 39c4 e0922008 e0a33009 e1c420f8 e1a05000 e3080644 e34c00e4 ebffc47c e5943018
[ 108.109705] 39e4 ee1d2f90 e7928003 e1a01005 e1a00004 e0886006 e7826003 eb1956b4 e3a00001
[ 108.118035]
[ 108.118035] LR: 0xc04e38fc:
[ 108.122310] 38fc e34ca110 e1a08000 e3e00000 ea000004 e79a2100 e5963018 e7933002 e0944003
[ 108.130644] 391c e0a55fc3 e2802001 e3a01004 e1a00007 ebff4dbe e5993000 e1500003 bafffff3
[ 108.138971] 393c e1a00006 e1a01008 eb1956e2 e1a00004 e1a01005 e8bd87f0 e92d43f8 e1a04000
[ 108.147303] 395c e3a00001 e1a06002 e1a07003 e59d5020 ebf1cf0d e3060160 e34c00e4 ebffc495
[ 108.155630] 397c e5943018 ee1d2f90 e7923003 e1a01fc5 e0968003 e0a79fc3 e1580005 e0d93001
[ 108.163965] 399c aa000004 e2652000 e1520008 e1a03fc2 e0d33009 ba00001f e1a00004 e0686006
[ 108.172292] 39bc eb19562b e1c420d8 e0922008 e0a33009 e1c420f8 e1a05000 e3080644 e34c00e4
[ 108.180627] 39dc ebffc47c e5943018 ee1d2f90 e7928003 e1a01005 e1a00004 e0886006 e7826003
[ 108.188956]
[ 108.188956] SP: 0xd2c09d68:
[ 108.193232] 9d68 c11045e4 c10a1b80 00000000 00000000 d2c09d98 00d7cbe2 00000000 d1554600
[ 108.201559] 9d88 c04e3984 20010093 ffffffff d2c09dd4 00000000 c010c018 00000000 c0e46160
[ 108.209893] 9da8 2de3e000 00000000 d27892e8 00000018 00000001 00000000 00000000 d1554600
[ 108.218221] 9dc8 d165eab0 00000008 00000000 d2c09de8 c04e397c c04e3984 20010093 ffffffff
[ 108.226555] 9de8 00000000 d27892c8 c11042b0 d50f01c0 a0010013 00000000 d1554600 c01f4368
[ 108.234885] 9e08 00000018 c0b39288 d50f01c0 d050eb6c d050eb7c c0261cd8 c780e400 00000000
[ 108.243220] 9e28 d27cc0e0 d27cc000 d301e800 c0332460 00000000 00000008 00000010 00000001
[ 108.251546] 9e48 d165ea50 00000000 b6a50070 d165eab0 00000000 00000001 0006c17c d301e800
[ 108.259878]
[ 108.259878] R1: 0xc0e460e0:
[ 108.264154] 60e0 20646162 76204350 65756c61 00000000 6f437325 203a6564 000a7325 61746146
[ 108.272483] 6100 7865206c 74706563 206e6f69 69206e69 7265746e 74707572 00000000 61746146
[ 108.280816] 6120 7865206c 74706563 006e6f69 73706f4f 62202d20 73206461 61637379 00006c6c
[ 108.289146] 6140 73706f4f 75202d20 6665646e 64656e69 736e6920 63757274 6e6f6974 00000000
[ 108.297482] 6160 64616572 00000000 74697277 00000065 61423201 6f6d2064 69206564 7325206e
[ 108.305808] 6180 6e616820 72656c64 74656420 65746365 00000a64 73706f4f 62202d20 6d206461
[ 108.314142] 61a0 0065646f 20646162 65646f6d 00000000 6e617262 74206863 756f7268 7a206867
[ 108.322470] 61c0 006f7265 73706f4f 62202d20 73206461 61637379 32286c6c 00000029 6e6b6e75
[ 108.330806]
[ 108.330806] R4: 0xd2789268:
[ 108.335081] 9268 00000000 00000000 00e56240 00000000 00000000 ffffffe0 d2789280 d2789280
[ 108.343411] 9288 c049badc 00000000 00000000 00000000 c121d5c2 c01461a8 d278927c ffffffff
[ 108.351738] 92a8 ffffffff 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 108.360068] 92c8 d285acd0 00200200 00000020 00000000 00000000 00000000 00000000 c0e58ec4
[ 108.368396] 92e8 00000000 00000000 00000000 00000000 00100100 00200200 00000000 00000000
[ 108.376727] 9308 00000000 00000000 00000000 00000000 00100100 00200200 00000000 00000000
[ 108.385058] 9328 00000000 00000000 00000000 00000000 00100100 00200200 00000000 00000000
[ 108.393389] 9348 00000000 00000000 00000000 00000000 00100100 00200200 00000000 00000000
[ 108.401719]
[ 108.401719] R9: 0xd1554580:
[ 108.405995] 4580 00000029 d1554540 d50f01c0 00000000 00d7cbe4 00000000 00000200 c780e800
[ 108.414330] 45a0 d050ea00 c0261adc 00000000 d15545ac d15545ac 00000000 00000000 00000000
[ 108.422655] 45c0 00000029 d1554580 d50f01c0 00000000 00d7cbe3 00000000 00000200 c780e600
[ 108.430988] 45e0 d050ea00 c0261adc 00000000 d15545ec d15545ec 00000000 00000000 00000000
[ 108.439315] 4600 0000002b d15545c0 d50f01c0 00000000 00d7cbe2 00000000 00000200 c780e400
[ 108.447647] 4620 d050ea00 c0261adc 00000000 d155462c d155462c 00000000 00000002 00000000
[ 108.455973] 4640 00000029 d1554600 d50f01c0 00000000 00d7cbe1 00000000 00000200 c780e200
[ 108.464307] 4660 d050ea00 c0261adc 00000000 d155466c d155466c 00000000 00000000 00000000
[ 108.472635]
[ 108.472635] R10: 0xd165ea30:
[ 108.476998] ea30 d165ea2c 00000000 000004d5 00000000 00000000 00000000 d165ea50 6f666e69
[ 108.485329] ea50 00020002 d165ea54 d165ea54 00000000 00000002 00ffffff 00000000 00000000
[ 108.493659] ea70 00000000 00000000 00000020 00000000 0d7cbe20 00000000 00000000 d27cc37c
[ 108.501989] ea90 00000000 00000000 00000000 d165ea9c d165ea9c 00000000 00000000 00000000
[ 108.510318] eab0 000341ff 000003ff 000003ff 00000000 ffffffff ffffffff c0c11140 d301e800
[ 108.518651] ead0 d165eb8c ccd7c150 00009313 00000000 00000000 00000000 00000000 00000000
[ 108.526980] eaf0 56e9f380 00000000 000004e0 00000000 000004e0 00000000 00090009 00000000
[ 108.535310] eb10 00000009 00000000 00000020 00000000 00000000 00000020 00000001 00000000
[ 108.543641] Process vold (pid: 228, stack limit = 0xd2c08210)
[ 108.549395] Stack: (0xd2c09de8 to 0xd2c0a000)
[ 108.553761] 9de0: 00000000 d27892c8 c11042b0 d50f01c0 a0010013 00000000
[ 108.561948] 9e00: d1554600 c01f4368 00000018 c0b39288 d50f01c0 d050eb6c d050eb7c c0261cd8
[ 108.570135] 9e20: c780e400 00000000 d27cc0e0 d27cc000 d301e800 c0332460 00000000 00000008
[ 108.578321] 9e40: 00000010 00000001 d165ea50 00000000 b6a50070 d165eab0 00000000 00000001
[ 108.586509] 9e60: 0006c17c d301e800 0006c17c d164ab28 b6a50070 c0331284 d0002088 d2c08000
[ 108.594695] 9e80: 7fffffff d2c08000 00000002 00000000 d165eb24 00000007 00000000 00000000
[ 108.602881] 9ea0: d2a6ce00 c016bab8 d2c09ea8 d165eab0 d165eb60 c0c10d00 c109fc64 00080400
[ 108.611067] 9ec0: d164ac88 c0332c0c d165eab0 c024c2c8 d164ac38 d165eab0 d164ac88 c0248878
[ 108.619254] 9ee0: 00000000 00000000 d164ac38 d153b660 d2c09f24 c0249068 00000003 d2c09f24
[ 108.627439] 9f00: d06abaa0 00000000 d2a6ce00 c01077c4 d2c08000 00000000 b6a50070 c02492c8
[ 108.635624] 9f20: d06abaa0 d164a970 d164ab08 00000003 d06abaa0 d301e800 00000000 c0249e08
[ 108.643810] 9f40: d301e800 00000083 c0c10d00 c0234fa8 d050ea00 00000083 c11da630 c02352a4
[ 108.651996] 9f60: d301e800 c11306fc c11da630 c0235588 d2a6ce00 d2fa2600 00000000 c024fa94
[ 108.660181] 9f80: d2a6d32c c014be94 d2fa261c d2c08000 c01077c4 d2c09fb0 00000034 c010af50
[ 108.668366] 9fa0: b69f2000 b68b0074 b68b0098 c010768c 00000000 00000008 00000014 00000073
[ 108.676552] 9fc0: b69f2000 b68b0074 b68b0098 00000034 b68b0080 b68b0058 b6883000 b6a50070
[ 108.684737] 9fe0: b68b008c b69bf6b8 7f60a4c7 b6c834cc 20010010 b69f2000 00000000 00000000
[ 108.692940] [<c04e3984>] (__percpu_counter_add) from [<c01f4368>] (account_page_dirtied+0x10c/0x178)
[ 108.702092] [<c01f4368>] (account_page_dirtied) from [<c0261cd8>] (__set_page_dirty+0x50/0xb8)
[ 108.710718] [<c0261cd8>] (__set_page_dirty) from [<c0332460>] (__fat_write_inode+0x158/0x220)
[ 108.719263] [<c0332460>] (__fat_write_inode) from [<c0331284>] (fat_truncate_blocks+0x264/0x32c)
[ 108.728060] [<c0331284>] (fat_truncate_blocks) from [<c0332c0c>] (fat_evict_inode+0x30/0x54)
[ 108.736512] [<c0332c0c>] (fat_evict_inode) from [<c024c2c8>] (evict+0x9c/0x150)
[ 108.743833] [<c024c2c8>] (evict) from [<c0248878>] (__dentry_kill+0x198/0x204)
[ 108.751066] [<c0248878>] (__dentry_kill) from [<c0249068>] (shrink_dentry_list+0x144/0x304)
[ 108.759428] [<c0249068>] (shrink_dentry_list) from [<c02492c8>] (shrink_dcache_parent+0x1c/0x60)
[ 108.768224] [<c02492c8>] (shrink_dcache_parent) from [<c0249e08>] (shrink_dcache_for_umount+0x2c/0xcc)
[ 108.777546] [<c0249e08>] (shrink_dcache_for_umount) from [<c0234fa8>] (generic_shutdown_super+0x1c/0xdc)
[ 108.787039] [<c0234fa8>] (generic_shutdown_super) from [<c02352a4>] (kill_block_super+0x18/0x68)
[ 108.795839] [<c02352a4>] (kill_block_super) from [<c0235588>] (deactivate_locked_super+0x58/0x7c)
[ 108.804727] [<c0235588>] (deactivate_locked_super) from [<c024fa94>] (cleanup_mnt+0x38/0x7c)
[ 108.813183] [<c024fa94>] (cleanup_mnt) from [<c014be94>] (task_work_run+0xb0/0xe8)
[ 108.820773] [<c014be94>] (task_work_run) from [<c010af50>] (do_work_pending+0x7c/0xa4)
[ 108.828703] [<c010af50>] (do_work_pending) from [<c010768c>] (work_pending+0xc/0x20)
[ 108.836456] Code: e34c00e4 ebffc495 e5943018 ee1d2f90 (e7923003)
[ 108.842557] ---[ end trace 27a65132658543fb ]---
[ 108.859918] Kernel panic - not syncing: Fatal exception
[ 108.865163] CPU3: stopping
[ 108.867886] CPU: 3 PID: 0 Comm: swapper/3 Tainted: G D 4.1.15 #72
[ 108.875116] Hardware name: Freescale i.MX6 Quad/DualLite (Device Tree)
[ 108.881667] [<c010f3e4>] (unwind_backtrace) from [<c010b554>] (show_stack+0x10/0x14)
[ 108.889429] [<c010b554>] (show_stack) from [<c0b30de4>] (dump_stack+0x84/0xc4)
[ 108.896667] [<c0b30de4>] (dump_stack) from [<c010e190>] (handle_IPI+0x33c/0x354)
[ 108.904074] [<c010e190>] (handle_IPI) from [<c0101484>] (gic_handle_irq+0x58/0x5c)
[ 108.911651] unwind: Unknown symbol address c0101484
[ 108.916536] unwind: Index not found c0101484
[ 108.920812] CPU2: stopping
[ 108.923534] CPU: 2 PID: 0 Comm: swapper/2 Tainted: G D 4.1.15 #72
[ 108.930764] Hardware name: Freescale i.MX6 Quad/DualLite (Device Tree)
[ 108.937310] [<c010f3e4>] (unwind_backtrace) from [<c010b554>] (show_stack+0x10/0x14)
[ 108.945067] [<c010b554>] (show_stack) from [<c0b30de4>] (dump_stack+0x84/0xc4)
[ 108.952302] [<c0b30de4>] (dump_stack) from [<c010e190>] (handle_IPI+0x33c/0x354)
[ 108.959709] [<c010e190>] (handle_IPI) from [<c0101484>] (gic_handle_irq+0x58/0x5c)
[ 108.967284] unwind: Unknown symbol address c0101484
[ 108.972167] unwind: Index not found c0101484
[ 108.976444] CPU1: stopping
[ 108.979167] CPU: 1 PID: 0 Comm: swapper/1 Tainted: G D 4.1.15 #72
[ 108.986396] Hardware name: Freescale i.MX6 Quad/DualLite (Device Tree)
[ 108.992940] [<c010f3e4>] (unwind_backtrace) from [<c010b554>] (show_stack+0x10/0x14)
[ 109.000698] [<c010b554>] (show_stack) from [<c0b30de4>] (dump_stack+0x84/0xc4)
[ 109.007933] [<c0b30de4>] (dump_stack) from [<c010e190>] (handle_IPI+0x33c/0x354)
[ 109.015341] [<c010e190>] (handle_IPI) from [<c0101484>] (gic_handle_irq+0x58/0x5c)
[ 109.022916] unwind: Unknown symbol address c0101484
[ 109.027799] unwind: Index not found c0101484
[ 109.045129] Rebooting in 5 seconds..

U-Boot 2015.04 (Jan 04 2017 - 17:44:22)

CPU: Freescale i.MX6Q rev1.5 at 792 MHz
CPU: Temperature 55 C
Reset cause: POR
Board: MX6-SabreSD
I2C: ready
DRAM: 2 GiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
*** Warning - bad CRC, using default environment

No panel detected: default to CPT
Display: CPT (960x1280)
WARNING: v_end_width (lower_margin) must be >= 2, adjusted
In: serial
Out: serial
Err: serial
check_and_clean: reg 0, flag_set 0
Fastboot: Normal
flash target is MMC:2
Net: Phy 1 not found
FEC [PRIME]
Error: FEC address not set.

Normal Boot

[ 6.573806] scsi 0:0:0:0: Direct-Access Kingston DTR30G2 PMAP PQ: 0 ANSI: 6
[ 6.996450] sd 0:0:0:0: [sda] 61472768 512-byte logical blocks: (31.4 GB/29.3 GiB)
[ 7.014707] sd 0:0:0:0: [sda] Write Protect is off
[ 7.021096] sd 0:0:0:0: [sda] No Caching mode page found
[ 7.034614] sd 0:0:0:0: [sda] Assuming drive cache: write through
[ 7.084766] sda: sda1
[ 7.109643] sd 0:0:0:0: [sda] Attached SCSI removable disk
[ 7.278139] healthd: No charger supplies found
[ 7.282653] healthd: No battery devices found
[ 7.625795] init: Service 'magd' (pid 231) exited with status 255
[ 7.696606] init: Starting service 'bootanim'...
[ 7.745597] init: Service 'flash_recovery' (pid 223) exited with status 0
[ 7.809676] ERROR: v4l2 capture: slave not found!
[ 7.824663] ERROR: v4l2 capture: slave not found!
[ 11.754705] init: Starting service 'gocsdk'...
[ 11.762162] init: Service 'gocsdk' (pid 475) exited with status 1
[ 11.768690] init: Service 'gocsdk' (pid 475) killing any children in process group
[ 12.447153] capability: warning: `main' uses 32-bit capabilities (legacy support in use)
[ 14.746302] zram: 536 (system_server) Attribute mem_used_total (and others) will be removed. See zram documentation.
[ 16.197222] random: nonblocking pool is initialized
[ 16.973659] init: Starting service 'gocsdk'...
[ 16.985087] init: Service 'gocsdk' (pid 561) exited with status 1
[ 16.991227] init: Service 'gocsdk' (pid 561) killing any children in process group
[ 20.548410] lowmemorykiller: lowmem_shrink: convert oom_adj to oom_score_adj:
[ 20.555711] lowmemorykiller: oom_adj 0 => oom_score_adj 0
[ 20.561187] lowmemorykiller: oom_adj 1 => oom_score_adj 58
[ 20.566782] lowmemorykiller: oom_adj 2 => oom_score_adj 117
[ 20.572436] lowmemorykiller: oom_adj 3 => oom_score_adj 176
[ 20.578091] lowmemorykiller: oom_adj 9 => oom_score_adj 529
[ 20.578096] lowmemorykiller: oom_adj 15 => oom_score_adj 1000
[ 21.114864] init: Starting service 'gocsdk'...
[ 21.127555] init: Service 'gocsdk' (pid 584) exited with status 1
[ 21.135812] init: Service 'gocsdk' (pid 584) killing any children in process group
[ 21.156777] init: Service 'bootanim' (pid 279) exited with status 0
[ 21.548936] acc_open
[ 21.551181] acc_release
[ 26.304284] init: Starting service 'gocsdk'...
[ 26.316518] init: Service 'gocsdk' (pid 911) exited with status 1
[ 26.323182] init: Service 'gocsdk' (pid 911) killing any children in process group
[ 27.465509] usb 1-1.4: USB disconnect, device number 4
[ 27.484769] sd 0:0:0:0: [sda] FAILED Result: hostbyte=DID_NO_CONNECT driverbyte=DRIVER_OK
[ 27.493003] sd 0:0:0:0: [sda] CDB: Read(10) 28 00 00 e0 12 a0 00 00 20 00
[ 27.493015] blk_update_request: I/O error, dev sda, sector 14684832
[ 27.512229] Buffer I/O error on dev sda1, logical block 1749220, async page read
[ 27.520599] Buffer I/O error on dev sda1, logical block 1749304, async page read
[ 27.532942] Buffer I/O error on dev sda1, logical block 1749340, async page read
[ 27.542982] Buffer I/O error on dev sda1, logical block 1749552, async page read
[ 27.551216] Buffer I/O error on dev sda1, logical block 1749692, async page read
[ 27.561053] Buffer I/O error on dev sda1, logical block 1749708, async page read
[ 27.569070] Buffer I/O error on dev sda1, logical block 1749912, async page read
[ 27.576920] Buffer I/O error on dev sda1, logical block 1750260, async page read
[ 27.586243] Buffer I/O error on dev sda1, logical block 1750552, async page read
[ 27.594080] Buffer I/O error on dev sda1, logical block 1750564, async page read
[ 27.604687] Unable to handle kernel paging request at virtual address 2de3e000
[ 27.611948] pgd = d34e8000
[ 27.614663] [2de3e000] *pgd=00000000
[ 27.618265] Internal error: Oops: 5 [#1] PREEMPT SMP ARM
[ 27.623583] Modules linked in:
[ 27.626665] CPU: 0 PID: 649 Comm: fsck_msdos Not tainted 4.1.15 #72
[ 27.632939] Hardware name: Freescale i.MX6 Quad/DualLite (Device Tree)
[ 27.639473] task: d28de600 ti: d34c6000 task.ti: d34c6000
[ 27.644891] PC is at __percpu_counter_add+0x30/0x104
[ 27.649865] LR is at __percpu_counter_add+0x28/0x104
[ 27.654837] pc : [<c04e3984>] lr : [<c04e397c>] psr: 200f0093
[ 27.654837] sp : d34c7d78 ip : 00000000 fp : 00001000
[ 27.666320] r10: d06b0e00 r9 : d527a3c0 r8 : 00000000
[ 27.671550] r7 : 00000000 r6 : 00000001 r5 : 00000018 r4 : d2d40108
[ 27.678083] r3 : 00000000 r2 : 2de3e000 r1 : c0e46160 r0 : 00000000
[ 27.684617] Flags: nzCv IRQs off FIQs on Mode SVC_32 ISA ARM Segment user
[ 27.691845] Control: 10c53c7d Table: 234e804a DAC: 00000015
[ 27.697595]
[ 27.697595] PC: 0xc04e3904:
[ 27.701870] 3904 e3e00000 ea000004 e79a2100 e5963018 e7933002 e0944003 e0a55fc3 e2802001
[ 27.710201] 3924 e3a01004 e1a00007 ebff4dbe e5993000 e1500003 bafffff3 e1a00006 e1a01008
[ 27.718529] 3944 eb1956e2 e1a00004 e1a01005 e8bd87f0 e92d43f8 e1a04000 e3a00001 e1a06002
[ 27.726855] 3964 e1a07003 e59d5020 ebf1cf0d e3060160 e34c00e4 ebffc495 e5943018 ee1d2f90
[ 27.735182] 3984 e7923003 e1a01fc5 e0968003 e0a79fc3 e1580005 e0d93001 aa000004 e2652000
[ 27.743509] 39a4 e1520008 e1a03fc2 e0d33009 ba00001f e1a00004 e0686006 eb19562b e1c420d8
[ 27.751836] 39c4 e0922008 e0a33009 e1c420f8 e1a05000 e3080644 e34c00e4 ebffc47c e5943018
[ 27.760162] 39e4 ee1d2f90 e7928003 e1a01005 e1a00004 e0886006 e7826003 eb1956b4 e3a00001
[ 27.768490]
[ 27.768490] LR: 0xc04e38fc:
[ 27.772765] 38fc e34ca110 e1a08000 e3e00000 ea000004 e79a2100 e5963018 e7933002 e0944003
[ 27.781092] 391c e0a55fc3 e2802001 e3a01004 e1a00007 ebff4dbe e5993000 e1500003 bafffff3
[ 27.789417] 393c e1a00006 e1a01008 eb1956e2 e1a00004 e1a01005 e8bd87f0 e92d43f8 e1a04000
[ 27.797745] 395c e3a00001 e1a06002 e1a07003 e59d5020 ebf1cf0d e3060160 e34c00e4 ebffc495
[ 27.806072] 397c e5943018 ee1d2f90 e7923003 e1a01fc5 e0968003 e0a79fc3 e1580005 e0d93001
[ 27.814399] 399c aa000004 e2652000 e1520008 e1a03fc2 e0d33009 ba00001f e1a00004 e0686006
[ 27.822725] 39bc eb19562b e1c420d8 e0922008 e0a33009 e1c420f8 e1a05000 e3080644 e34c00e4
[ 27.831051] 39dc ebffc47c e5943018 ee1d2f90 e7928003 e1a01005 e1a00004 e0886006 e7826003
[ 27.839379]
[ 27.839379] SP: 0xd34c7cf8:
[ 27.843654] 7cf8 00000001 d30c0048 eeeecbc0 d30c0048 d28de648 d30c0048 eeeecbc0 c0161668
[ 27.851980] 7d18 c04e3984 200f0093 ffffffff d34c7d64 00000000 c010c018 00000000 c0e46160
[ 27.860307] 7d38 2de3e000 00000000 d2d40108 00000018 00000001 00000000 00000000 d527a3c0
[ 27.868633] 7d58 d06b0e00 00001000 00000000 d34c7d78 c04e397c c04e3984 200f0093 ffffffff
[ 27.876961] 7d78 00000000 d2d400e8 c11042b0 d527a3c0 a00f0013 00000000 d527a3c0 c01f4368
[ 27.885290] 7d98 00000018 c0b39288 d527a3c0 d001276c d001277c c0261cd8 00000000 00000000
[ 27.893617] 7db8 00001000 d06b0e00 00001000 c0262e00 00001000 00000000 00001000 00001000
[ 27.901942] 7dd8 d0012690 00001000 00000000 d2dc76c0 c0c08ac4 c0262e8c 00000001 d527a3c0
[ 27.910269]
[ 27.910269] R1: 0xc0e460e0:
[ 27.914544] 60e0 20646162 76204350 65756c61 00000000 6f437325 203a6564 000a7325 61746146
[ 27.922871] 6100 7865206c 74706563 206e6f69 69206e69 7265746e 74707572 00000000 61746146
[ 27.931196] 6120 7865206c 74706563 006e6f69 73706f4f 62202d20 73206461 61637379 00006c6c
[ 27.939524] 6140 73706f4f 75202d20 6665646e 64656e69 736e6920 63757274 6e6f6974 00000000
[ 27.947852] 6160 64616572 00000000 74697277 00000065 61423201 6f6d2064 69206564 7325206e
[ 27.956179] 6180 6e616820 72656c64 74656420 65746365 00000a64 73706f4f 62202d20 6d206461
[ 27.964506] 61a0 0065646f 20646162 65646f6d 00000000 6e617262 74206863 756f7268 7a206867
[ 27.972833] 61c0 006f7265 73706f4f 62202d20 73206461 61637379 32286c6c 00000029 6e6b6e75
[ 27.981160]
[ 27.981160] R4: 0xd2d40088:
[ 27.985435] 0088 00000000 00000000 00e245c8 00000000 00000000 ffffffe0 d2d400a0 d2d400a0
[ 27.993763] 00a8 c049badc 00000000 00200200 ffff958c eef02402 c01461a8 d2d4009c ffffffff
[ 28.002089] 00c8 ffffffff 00000000 00000000 00000000 00000000 00000000 d2214500 00000003
[ 28.010415] 00e8 d2be2cd0 00200200 00000020 00000000 00000000 00000000 00000000 c0e58ec4
[ 28.018741] 0108 00000000 00000000 00000000 00000000 00100100 00200200 00000000 00000000
[ 28.027068] 0128 00000000 00000000 00000000 00000000 00100100 00200200 00000000 00000000
[ 28.035394] 0148 00000000 00000000 00000000 00000000 00100100 00200200 00000000 00000000
[ 28.043721] 0168 00000000 00000000 00000000 00000000 00100100 00200200 00000000 00000000
[ 28.052050]
[ 28.052050] R9: 0xd527a340:
[ 28.056325] a340 00000802 d001276c 001ab6c0 ffffffff 00000003 00100100 00200200 d06b0dc0
[ 28.064651] a360 00000822 d001276c 001a8700 ffffffff 00000002 d527a474 d527b854 d073ea80
[ 28.072978] a380 00000000 00000000 00000000 ffffffff 00000001 00100100 00200200 00dc00dc
[ 28.081304] a3a0 00000822 d001276c 001a6f7c ffffffff 00000002 d527cff4 d5180d14 d073e5c0
[ 28.089631] a3c0 00000815 d001276c 001a66a0 ffffffff 00000004 00100100 00200200 d06b0e00
[ 28.097957] a3e0 00000000 00000000 00000000 ffffff80 00000000 d527a9d4 d527ab94 00000000
[ 28.106284] a400 00000000 00000000 00000000 ffffffff 00000001 00100100 00200200 00040004
[ 28.114611] a420 00000000 00000000 00000000 ffffffff 00000001 00100100 00200200 00070007
[ 28.122938]
[ 28.122938] R10: 0xd06b0d80:
[ 28.127300] 0d80 00000028 d06b0d80 d527b260 00000000 001ab638 00000000 00001000 d3d93000
[ 28.135628] 0da0 d0012600 c02629bc 00000000 d06b0dac d06b0dac 00000000 00000000 00000000
[ 28.143953] 0dc0 00000028 d06b0dc0 d527a340 00000000 001ab6c0 00000000 00001000 d3d1a000
[ 28.152281] 0de0 d0012600 c02629bc 00000000 d06b0dec d06b0dec 00000000 00000000 00000000
[ 28.160606] 0e00 00000023 d06b0e00 d527a3c0 00000000 001a66a0 00000000 00001000 d3d1e000
[ 28.168935] 0e20 d0012600 00000000 00000000 d06b0e2c d06b0e2c 00000000 00000000 00000000
[ 28.177260] 0e40 d06b0e80 d06b0e60 d06b0dc0 00000d2c 00000001 00000000 0001d9ad 08000000
[ 28.185587] 0e60 d06b0e40 00000000 00000000 00000d30 00000001 00000020 0001d9b1 08000000
[ 28.193916] Process fsck_msdos (pid: 649, stack limit = 0xd34c6210)
[ 28.200189] Stack: (0xd34c7d78 to 0xd34c8000)
[ 28.204553] 7d60: 00000000 d2d400e8
[ 28.212739] 7d80: c11042b0 d527a3c0 a00f0013 00000000 d527a3c0 c01f4368 00000018 c0b39288
[ 28.220925] 7da0: d527a3c0 d001276c d001277c c0261cd8 00000000 00000000 00001000 d06b0e00
[ 28.229110] 7dc0: 00001000 c0262e00 00001000 00000000 00001000 00001000 d0012690 00001000
[ 28.237296] 7de0: 00000000 d2dc76c0 c0c08ac4 c0262e8c 00000001 d527a3c0 00001000 d001276c
[ 28.245482] 7e00: 00001000 c0266dcc 00001000 00001000 d527a3c0 c024c01c 00001000 00001000
[ 28.253667] 7e20: d34c7f1c c01ea878 00001000 00001000 d527a3c0 c024c01c a66a0000 00000001
[ 28.261852] 7e40: d2133b50 00000000 d34c6000 00000000 d527a3c0 c024c01c 0000023b 00000000
[ 28.270037] 7e60: d34c7f30 00000000 d2dc76c0 d2dc76c0 d34c7f1c d001276c b6d0f000 c01ec3c0
[ 28.278222] 7e80: 00000002 c0542b7c 00000001 00000001 00000000 d36b4f8c 200f0013 94180000
[ 28.286408] 7ea0: 00000005 d34c7f30 d2dc76c0 d34c7f1c d34c6000 00000000 b6d0f000 c0267270
[ 28.294594] 7ec0: d0594d70 d36b4e00 d34c6000 c0b394fc d34c7ed0 d34c7ed0 d34c7ed8 d34c7ed8
[ 28.302779] 7ee0: d34c7ee0 d34c7ee0 c123a768 d2dc76c0 00004000 a66a0000 00000001 d34c7f88
[ 28.310966] 7f00: d34c6000 c0233150 00004000 00000002 a66a0000 b6d0b000 00004000 00000001
[ 28.319151] 7f20: 00000000 00004000 d34c7f14 00000001 d2dc76c0 00000000 a66a0000 00000001
[ 28.327336] 7f40: 00000000 00000000 00000000 00000000 d2dc76c0 00004000 b6d0b000 d34c7f88
[ 28.335521] 7f60: c01077c4 c02338e8 00000008 00000000 d2dc76c0 d2dc76c0 00004000 b6d0b000
[ 28.343707] 7f80: c01077c4 c0234110 a66a0000 00000001 00000200 00004000 b6d0f000 7f5ea110
[ 28.351893] 7fa0: 00000004 c0107640 00004000 b6d0f000 00000003 b6d0b000 00004000 bed466f0
[ 28.360078] 7fc0: 00004000 b6d0f000 7f5ea110 00000004 b6d0f020 00000001 b655f4c0 b6d0f000
[ 28.368263] 7fe0: 00000001 bed46700 7f5e3b6f b6e4c5d4 600f0010 00000003 32161d25 fc2c0060
[ 28.376466] [<c04e3984>] (__percpu_counter_add) from [<c01f4368>] (account_page_dirtied+0x10c/0x178)
[ 28.385618] [<c01f4368>] (account_page_dirtied) from [<c0261cd8>] (__set_page_dirty+0x50/0xb8)
[ 28.394245] [<c0261cd8>] (__set_page_dirty) from [<c0262e00>] (__block_commit_write+0x90/0xb8)
[ 28.402869] [<c0262e00>] (__block_commit_write) from [<c0262e8c>] (block_write_end+0x40/0x80)
[ 28.411406] [<c0262e8c>] (block_write_end) from [<c0266dcc>] (blkdev_write_end+0x28/0x48)
[ 28.419599] [<c0266dcc>] (blkdev_write_end) from [<c01ea878>] (generic_perform_write+0x120/0x1b8)
[ 28.428487] [<c01ea878>] (generic_perform_write) from [<c01ec3c0>] (__generic_file_write_iter+0x164/0x1b4)
[ 28.438152] [<c01ec3c0>] (__generic_file_write_iter) from [<c0267270>] (blkdev_write_iter+0x98/0x138)
[ 28.447386] [<c0267270>] (blkdev_write_iter) from [<c0233150>] (__vfs_write+0xa8/0xd8)
[ 28.455316] [<c0233150>] (__vfs_write) from [<c02338e8>] (vfs_write+0x90/0x164)
[ 28.462636] [<c02338e8>] (vfs_write) from [<c0234110>] (SyS_write+0x44/0x9c)
[ 28.469702] [<c0234110>] (SyS_write) from [<c0107640>] (ret_fast_syscall+0x0/0x3c)
[ 28.477281] Code: e34c00e4 ebffc495 e5943018 ee1d2f90 (e7923003)
[ 28.483383] ---[ end trace bb3b5ff321d78363 ]---
[ 28.500966] Kernel panic - not syncing: Fatal exception
[ 28.506212] CPU3: stopping
[ 28.508937] CPU: 3 PID: 0 Comm: swapper/3 Tainted: G D 4.1.15 #72
[ 28.516166] Hardware name: Freescale i.MX6 Quad/DualLite (Device Tree)
[ 28.522718] [<c010f3e4>] (unwind_backtrace) from [<c010b554>] (show_stack+0x10/0x14)
[ 28.530481] [<c010b554>] (show_stack) from [<c0b30de4>] (dump_stack+0x84/0xc4)
[ 28.537718] [<c0b30de4>] (dump_stack) from [<c010e190>] (handle_IPI+0x33c/0x354)
[ 28.545127] [<c010e190>] (handle_IPI) from [<c0101484>] (gic_handle_irq+0x58/0x5c)
[ 28.552702] unwind: Unknown symbol address c0101484
[ 28.557585] unwind: Index not found c0101484
[ 28.561862] CPU1: stopping
[ 28.564587] CPU: 1 PID: 0 Comm: swapper/1 Tainted: G D 4.1.15 #72
[ 28.571816] Hardware name: Freescale i.MX6 Quad/DualLite (Device Tree)
[ 28.578362] [<c010f3e4>] (unwind_backtrace) from [<c010b554>] (show_stack+0x10/0x14)
[ 28.586119] [<c010b554>] (show_stack) from [<c0b30de4>] (dump_stack+0x84/0xc4)
[ 28.593354] [<c0b30de4>] (dump_stack) from [<c010e190>] (handle_IPI+0x33c/0x354)
[ 28.600762] [<c010e190>] (handle_IPI) from [<c0101484>] (gic_handle_irq+0x58/0x5c)
[ 28.608336] unwind: Unknown symbol address c0101484
[ 28.613219] unwind: Index not found c0101484
[ 28.617496] CPU2: stopping
[ 28.620219] CPU: 2 PID: 0 Comm: swapper/2 Tainted: G D 4.1.15 #72
[ 28.627448] Hardware name: Freescale i.MX6 Quad/DualLite (Device Tree)
[ 28.633993] [<c010f3e4>] (unwind_backtrace) from [<c010b554>] (show_stack+0x10/0x14)
[ 28.641751] [<c010b554>] (show_stack) from [<c0b30de4>] (dump_stack+0x84/0xc4)
[ 28.648987] [<c0b30de4>] (dump_stack) from [<c010e190>] (handle_IPI+0x33c/0x354)
[ 28.656394] [<c010e190>] (handle_IPI) from [<c0101484>] (gic_handle_irq+0x58/0x5c)
[ 28.663968] unwind: Unknown symbol address c0101484
[ 28.668851] unwind: Index not found c0101484
[ 28.686446] Rebooting in 5 seconds..

U-Boot 2015.04 (Jan 04 2017 - 17:44:22)

CPU: Freescale i.MX6Q rev1.5 at 792 MHz
CPU: Temperature 61 C
Reset cause: POR
Board: MX6-SabreSD
I2C: ready
DRAM: 2 GiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
*** Warning - bad CRC, using default environment

No panel detected: default to CPT
Display: CPT (960x1280)
WARNING: v_end_width (lower_margin) must be >= 2, adjusted
In: serial
Out: serial
Err: serial
check_and_clean: reg 0, flag_set 0
Fastboot: Normal

0 项奖励
回复
4 回复数

2,475 次查看
小小原子
Contributor II

I also met this  problem in Linux "rel_imx_4.1.15_2.1.0_ga" downloaded from "linux-imx.git - i.MX Linux Kernel ". It almost  took me one week to find way to fix this problem. And finally, I found the answer in "https://patchwork.kernel.org/patch/9363667/". I wish this could help more people that met the same problem.

2,475 次查看
gengde_zheng
Contributor I

thank you very much.i also met this  problem  and have fixed it as you said.

0 项奖励
回复

2,475 次查看
TimPearce
Contributor IV

You may also with to try the following kernel patch:

Google Groups 

I have not tested this change myself, but the issue appears similar re: crash. The errors preceding the crash would likely be a different issue though.

Tim

0 项奖励
回复

2,475 次查看
igorpadykov
NXP Employee
NXP Employee

Hi

kernel panic may be caused also hardware issues, please recheck

memory with ddr test

https://community.freescale.com/docs/DOC-105652 

and check usb subsystem with linux unit tests (imx-test../mxc_usb_test)
www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复