android kernel version change(imx8mqevk)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

android kernel version change(imx8mqevk)

2,598 Views
dngnstjd
Contributor II

Hi, I am porting android OS to imx8 processor board now.

Currently, The Android version I am using is Oreo and the kernel version is 4.9.88(imx-o8.1.0_1.3.0)

I want to change the kernel version to 4.14

Because, I have to use SPI.

However, after changing the kernel version and proceeding with the build an error occurred.

"FAILED: out/target /product/evk_8mq/vbmeta.img"

"/bin/bash -c "for dtsplat in imx8mq:fsl-imx8mq-evk.dtb; do DTS_PLATFORM=\`echo \$dtsplat | cut -d':' -f1\`; VBMETA_IMAGE_BOARD=out/target/product/evk_8mq/vbmeta-\$DTS_PLATFORM.img; out/host/linux-x86/bin/avbtool make_vbmeta_image --include_descriptors_from_image out/target/product/evk_8mq/boot-\$DTS_PLATFORM.img --include_descriptors_from_image out/target/product/evk_8mq/system.img --include_descriptors_from_image out/target/product/evk_8mq/vendor.img --algorithm SHA256_RSA4096 --key external/avb/test/data/testkey_rsa4096.pem --padding_size 4096 --output \$VBMETA_IMAGE_BOARD ; done"
out/host/linux-x86/bin/avbtool: Given image does not look like a vbmeta image.
ninja: build stopped: subcommand failed."

I wonder why this error occurs???

Thank you!!!

 

Tags (1)
0 Kudos
Reply
1 Reply

2,593 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello dngnstjd,

 

You have to adjust and compile the device tree at 4.14v, since you are changing kernel version.

 

Regards

0 Kudos
Reply