Starting up ecspi1 on a imx8mm smarc module

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Starting up ecspi1 on a imx8mm smarc module

789件の閲覧回数
joost
Contributor I

Hi,

My problem is basically the same as in https://community.nxp.com/t5/i-MX-Processors/Enabling-ecspi1-on-imx8mm-isn-t-working/m-p/1218229 , but that solution doesn't seem to work for me. So I hope somebody has a hint.

I'm using a Congatec imx8mm smarc module and I want to use its ECSPI1 interface. I'm using the 5.4.47 kernel from Congatec, but I also tried a (patched) 5.10.72 version from NXP. But in both kernels I can't get it running.

In the 5.10 kernel I can see - when using an oscilloscope - the correct chip select lines going low when I try to send some data to a slave. But I cannot see any clock signal or signals on the MISO an MOSI lines. In the 5.4 kernel I cannot see anything happening at all.

We have two microchip ksz8895 switches connected to the spi bus. I added the first in the device tree, and the second as a spidev device for further testing.

 

I used the following device tree entries:

pinctrl_ecspi1: ecspi1grp {
    fsl,pins = <
        MX8MM_IOMUXC_ECSPI1_SCLK_ECSPI1_SCLK 0x150
        MX8MM_IOMUXC_ECSPI1_MOSI_ECSPI1_MOSI 0x150
        MX8MM_IOMUXC_ECSPI1_SS0_ECSPI1_SS0 0x150
        MX8MM_IOMUXC_ECSPI1_MISO_ECSPI1_MISO 0x150
    >;
};

&ecspi1 {
        status = "okay";
        pinctrl-names = "default";
        pinctrl-0 = <&pinctrl_ecspi1>;
        cs-gpios = <&gpio4 10 GPIO_ACTIVE_LOW>, <&gpio4 20 GPIO_ACTIVE_LOW>;
        num-cs = <2>;
        id = <1>;
        spi-cpha;
        spi-cpol;

       ksz8795a: ksz8795@0 {
            status = "okay";
            compatible = "microchip,ksz8795";
            reg = <0>;
            dsa,member = <0 0>;

            spi-max-frequency = <12500000>;
            spi-cpha;
            spi-cpol;

            ports {
                #address-cells = <1>;
                #size-cells = <0>;
                port@0 {
                    reg = <0>;
                    label = "lan01";
                };
                port@1 {
                    reg = <1>;
                    label = "lan02";
                };
                port@2 {
                    reg = <2>;
                    label = "lan03";
                };
                port@3 {
                    reg = <3>;
                    label = "lan04";
                };
                port@4 {
                    reg = <4>;
                    label = "lan05";
                };
                port@5 {
                    reg = <5>;
                    label = "lan9500";
                    //ethernet = <&eth1>;
                    fixed-link {
                        speed = <100>;
                        full-duplex;
                    };
                };
            };
        };

    switch1: spidev@1 {
        compatible = "spidev";
        spi-max-frequency = <12500000>;
        reg = <1>;
        status = "okay";
    };
};

 

The pinctrl-handles seem to be ok (30820000 = ecspi1):

cat /sys/kernel/debug/pinctrl/pinctrl-handles 

device: 30820000.spi current state: default
  state: default
    type: MUX_GROUP controller 30330000.pinctrl group: ecspi1grp (21) function: pinctrl (0)
    type: CONFIGS_PIN controller 30330000.pinctrl pin MX8MM_IOMUXC_ECSPI1_SCLK (125)config 00000150
    type: CONFIGS_PIN controller 30330000.pinctrl pin MX8MM_IOMUXC_ECSPI1_MOSI (126)config 00000150
    type: CONFIGS_PIN controller 30330000.pinctrl pin MX8MM_IOMUXC_ECSPI1_SS0 (128)config 00000150
    type: CONFIGS_PIN controller 30330000.pinctrl pin MX8MM_IOMUXC_ECSPI1_MISO (127)config 00000150

gpioinfo gives me the following:

gpioinfo

gpiochip3 - 32 lines:
        line  10:      unnamed   "spi0 CS0"  output   active-low [used]
        line  20:      unnamed   "spi0 CS1"  output   active-low [used]

 

But when trying to send some data I'll get an IO Error. When monitoring with an oscilloscope I can only see the chip select line going down. No clock, miso or mosi.

./spidev_test -D /dev/spidev0.1 -s 12500000 -v

output in kernel log:
[ 2161.215336] spidev spi0.1: spi_imx_setup: mode 4, 8 bpw, 12500000 hz
[ 2161.215366] spidev spi0.1: setup mode 0, cs_high, 8 bits/w, 12500000 Hz max --> 0
[ 2161.215374] spidev spi0.1: spi mode 4
[ 2161.215384] spidev spi0.1: spi_imx_setup: mode 4, 8 bpw, 12500000 hz
[ 2161.215393] spidev spi0.1: setup mode 0, cs_high, 8 bits/w, 12500000 Hz max --> 0
[ 2161.215401] spidev spi0.1: 8 bits per word
[ 2161.215408] spidev spi0.1: spi_imx_setup: mode 4, 8 bpw, 12500000 hz
[ 2161.215418] spidev spi0.1: setup mode 0, cs_high, 8 bits/w, 12500000 Hz max --> 0
[ 2161.215426] spidev spi0.1: 12500000 Hz (max)
[ 2161.215596] spi_imx 30820000.spi: mx51_ecspi_clkdiv: fin: 50000000, fspi: 12500000, post: 0, pre: 3
[ 2163.230524] spidev spi0.1: I/O Error in PIO
[ 2163.230542] spidev spi0.1: SPI transfer failed: -110
[ 2163.230566] spi_master spi0: failed to transfer one message from queue

 

Loading the ksz8795-spi drivers, gives me the same error.

Does anybody has an idea what I missed or where to look for?

0 件の賞賛
返信
0 返答(返信)