android camera application not working on imx53 smd custom board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

android camera application not working on imx53 smd custom board

2,668 次查看
Rajput1z
Contributor II

Hi all,

       I'm using custom board based on i.MX53 smd, and Android r10.4. I'm trying to get ov (csi interface )camera to work.

           also /dev/video0 is created ,but when I try to open system application "Camera", i have exception:

I/ActivityManager( 2170): Starting: Intent { act=android.intent.action.MAIN cat=[android.intent.category.LAUNCHER] flg=0x10200000 cmp=com.android.camera/.Camera bnds=[599,25][685,99] } from pid 2240

I/SurfaceFlinger( 2170): mHw->getFormat() 5

I/ActivityManager( 2170): Start proc com.android.camera for activity com.android.camera/.Camera: pid=2457 uid=10021 gids={1006, 1015}

V/AudioPolicyManagerBase( 2129): stopOutput() output 1, stream 1, session 4

V/AudioPolicyManagerBase( 2129): changeRefCount() stream 1, count 0

V/AudioPolicyManagerBase( 2129): getNewDevice() selected device 0

V/AudioPolicyManagerBase( 2129): setOutputDevice() output 1 device 0 delayMs 0

V/AudioPolicyManagerBase( 2129): setOutputDevice() setting same device 0 or null device for output 1

W/dalvikvm( 2457): Exception Ljava/lang/NullPointerException; thrown while initializing Lcom/android/camera/CameraSettings;

D/AndroidRuntime( 2457): Shutting down VM

W/dalvikvm( 2457): threadid=1: thread exiting with uncaught exception (group=0x40015560)

E/AndroidRuntime( 2457): FATAL EXCEPTION: main

E/AndroidRuntime( 2457): java.lang.ExceptionInInitializerError

E/AndroidRuntime( 2457):     at com.android.camera.Camera.onCreate(Camera.java:891)

E/AndroidRuntime( 2457):     at android.app.Instrumentation.callActivityOnCreate(Instrumentation.java:1047)

E/AndroidRuntime( 2457):     at android.app.ActivityThread.performLaunchActivity(ActivityThread.java:1611)

E/AndroidRuntime( 2457):     at android.app.ActivityThread.handleLaunchActivity(ActivityThread.java:1663)

E/AndroidRuntime( 2457):     at android.app.ActivityThread.access$1500(ActivityThread.java:117)

E/AndroidRuntime( 2457):     at android.app.ActivityThread$H.handleMessage(ActivityThread.java:931)

E/AndroidRuntime( 2457):     at android.os.Handler.dispatchMessage(Handler.java:99)

E/AndroidRuntime( 2457):     at android.os.Looper.loop(Looper.java:130)

E/AndroidRuntime( 2457):     at android.app.ActivityThread.main(ActivityThread.java:3683)

E/AndroidRuntime( 2457):     at java.lang.reflect.Method.invokeNative(Native Method)

E/AndroidRuntime( 2457):     at java.lang.reflect.Method.invoke(Method.java:507)

E/AndroidRuntime( 2457):     at com.android.internal.os.ZygoteInit$MethodAndArgsCaller.run(ZygoteInit.java:839)

E/AndroidRuntime( 2457):     at com.android.internal.os.ZygoteInit.main(ZygoteInit.java:597)

E/AndroidRuntime( 2457):     at dalvik.system.NativeStart.main(Native Method)

E/AndroidRuntime( 2457): Caused by: java.lang.NullPointerException

E/AndroidRuntime( 2457):     at com.android.camera.CameraSettings.<clinit>(CameraSettings.java:63)

E/AndroidRuntime( 2457):     ... 14 more

W/ActivityManager( 2170):   Force finishing activity com.android.camera/.Camera

W/ActivityManager( 2170): Activity pause timeout for HistoryRecord{40733300 com.android.camera/.Camera}

even  I'm trying to get UVC camera to work , in this case also i am getting same error , please suggest me how to resolve this issue .

Regards,

Rajput

标签 (2)
0 项奖励
回复
4 回复数

2,249 次查看
ToxicAvenger
Contributor III

Hello,

I have similar problem. I removed default camera apk and use android-webcam/android-webcam-library at master · openxc/android-webcam · GitHub

Regards,

Toxic

0 项奖励
回复

2,249 次查看
Rajput1z
Contributor II

Thank you for reply Toxic,

   the link which you provided is work only USB base webcam , will it work for inbuilt cam?  in my case my board is having internal camera (csi interface ) , and i am using ov5642 driver for it.

so, plz suggest me on this case .

Regards,

Rajput

0 项奖励
回复

2,249 次查看
Rajput1z
Contributor II

plz anyone help me to resolve this exception :smileyplain:

0 项奖励
回复

2,249 次查看
ToxicAvenger
Contributor III

Im not sure, just try it :-)

0 项奖励
回复