What kind of SD card is compatible with the iMX6 DualLite processor.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What kind of SD card is compatible with the iMX6 DualLite processor.

ソリューションへジャンプ
1,734件の閲覧回数
gvdbe_fr
Contributor I

Hello

I bought a Wandboard card with the iMX6 DualLite Processor.

I would like to know which SD card is compatible with the iMX6 DualLite processor. (CAT 4/6/8/10 ?)

Wandboard forums community seems doesn't know.

Could you help me ?

Regards.

:smileyblush:

ラベル(1)
0 件の賞賛
返信
1 解決策
1,578件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

You can go to http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6DL&fpsp=1&tab=Documentation_Tabto download i.MX6DL reference manual. In the chapters 1.4 and 67.1 of the i.MX6SDLRM you can find which SD card is compatible with the iMX6 DualLite processor.

Best Regards

Dan

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,579件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

You can go to http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6DL&fpsp=1&tab=Documentation_Tabto download i.MX6DL reference manual. In the chapters 1.4 and 67.1 of the i.MX6SDLRM you can find which SD card is compatible with the iMX6 DualLite processor.

Best Regards

Dan

0 件の賞賛
返信
1,578件の閲覧回数
gvdbe_fr
Contributor I

Fine !

Thanks you

Best regards

Guy

On Mon, 16 Sep 2013 23:34:08 -0700, Dan Wang

0 件の賞賛
返信