android booting issue with SABRE-SD 6DQ

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

android booting issue with SABRE-SD 6DQ

2,117 次查看
waynelou
Contributor I

Hello,

 

I am working on imx6 sabre-sd 6dq with Android 4.4. Now I am porting TI's wifi module(WL18xx) to the board.

Before I insert the wireless card to the board, I could boot normally.

But when I insert the wireless card to the board, it would have binder issue and I could not get into Android desktop enviroment successfully.

I could see below binder issue on boot log,

And I also attached entire booting log, please give me some clues to solve this issue.

Thank you very much!


ehci_fsl_bus_suspend begins, Host 1

ehci_fsl_bus_suspend ends, Host 1

binder: release 2663:2674 transaction 4960 in, still active

binder: send failed reply for transaction 4960 to 2886:2886

binder: release 2663:2779 transaction 4955 in, still active

binder: send failed reply for transaction 4955 to 2886:2936

binder: release 2663:2780 transaction 4959 in, still active

binder: send failed reply for transaction 4959 to 2872:2872

binder: send failed reply for transaction 4965 to 2728:2728

binder: send failed reply for transaction 4978 to 2310:2687

binder: send failed reply for transaction 5095 to 2872:2951

binder: send failed reply for transaction 5096 to 2872:2953

binder: send failed reply for transaction 5097 to 2872:2955

binder: send failed reply for transaction 5102 to 2872:2954

binder: send failed reply for transaction 5103 to 2872:2952

binder: release proc 2663, transaction 5152, not freed

binder: 2886:2886 transaction failed 29189, size 272-0

binder: 2886:2936 transaction failed 29189, size 116-0

binder: 2728:2728 transaction failed 29189, size 172-0

alarm_release: clear alarm, pending 0

alarm_release: clear alarm, pending 0

binder: 2899:2899 transaction failed 29189, size 76-0

request_suspend_state: wakeup (0->0) at 31945095673 (1970-01-02 00:00:16.124120336 UTC)

init: untracked pid 2899 exited

init: untracked pid 2872 exited

init: untracked pid 2845 exited

init: untracked pid 2858 exited

init: untracked pid 2925 exited

init: untracked pid 2959 exited

init: untracked pid 2767 exited

ERROR: v4l2 capture: slave not found!

ERROR: v4l2 capture: slave not found!

ERROR: v4l2 capture: slave not found!

ERROR: v4l2 capture: slave not found!

ERROR: v4l2 capture: slave not found!

ERROR: v4l2 capture: slave not found!

ERROR: v4l2 capture: slave not found!

ERROR: v4l2 capture: slave not found!

SELinux: initialized (dev tmpfs, type tmpfs), uses transition SIDs

mma enable setting inactive

period -1547481011 ,timeout is 702124073, wake up is

period -1547481011 ,timeout is 702124073, wake up is

request_suspend_state: wakeup (0->0) at 37682373673 (1970-01-02 00:00:21.861400002 UTC)

period 66 ,timeout is 0, wake up is

mma enable setting active

remove wake up source irq 110

 

 

Regards,

Wayne

Original Attachment has been moved to: android_binder_issue.txt.zip

标签 (2)
0 项奖励
回复
2 回复数

1,150 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Wayne

for binding suggest to look below

wifi binding on imx6sl evk based board

wilink8 (wl1835mod) patches for imx6SL with 3.10.17 kernel

http://e2e.ti.com/support/wireless_connectivity/f/307/t/361507.aspx

Best regards

igor

0 项奖励
回复

1,150 次查看
haoranwang
NXP Employee
NXP Employee

Hi Wayne,

    

     1. Could you provide the whole logcat by use "logcat -v time"? The hung log of binder seems Android BSP HAL has some issue with your wifi.

     2. Please provide your Android BSP version from the "settings --> about tablet".

    

BRs

Haoran

0 项奖励
回复