Can the IMX6Q output the LVDS video in only one pair Differential signal?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can the IMX6Q output the LVDS video in only one pair Differential signal?

Jump to solution
1,168 Views
翔李
Contributor IV

Hi, can the IMX6Q output the LVDS video in only one pair Differential signal?  Because the monitor which the IMX6Q board connects,has only one pari Differential signal interface. Thanks.

Labels (1)
0 Kudos
Reply
1 Solution
1,048 Views
igorpadykov
NXP Employee
NXP Employee

Hi 翔 李

unfortunately not, this is fixed in hardware. From

IMX6DQRM Table 39-1. LDB - Block Description :

LDB has 2 channel serializers. The serializer does parallel to serial conversion 7:1 to

3 or 4 data lines

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,049 Views
igorpadykov
NXP Employee
NXP Employee

Hi 翔 李

unfortunately not, this is fixed in hardware. From

IMX6DQRM Table 39-1. LDB - Block Description :

LDB has 2 channel serializers. The serializer does parallel to serial conversion 7:1 to

3 or 4 data lines

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply