android add new apn

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

android add new apn

2,043 Views
marekbil
Contributor I

I can't add new apn, i have message "Access Point Name settings are not available for this user".

Labels (1)
0 Kudos
Reply
2 Replies

1,844 Views
marekbil
Contributor I

I have apns-conf.xml in etc but not working

0 Kudos
Reply

1,844 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Maker,

You could refer to the following thread, which seems to be a similar case and it is already answered:

APN List is Empty in Android ICS imx6

Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply