android add new apn

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

android add new apn

2,046件の閲覧回数
marekbil
Contributor I

I can't add new apn, i have message "Access Point Name settings are not available for this user".

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,847件の閲覧回数
marekbil
Contributor I

I have apns-conf.xml in etc but not working

0 件の賞賛
返信

1,847件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Maker,

You could refer to the following thread, which seems to be a similar case and it is already answered:

APN List is Empty in Android ICS imx6

Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信