an error was encountered while installing and opening project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

an error was encountered while installing and opening project

1,199 Views
melanie
Contributor III

Hi 

Q1:I already have version 11.6 installed, can I install version 11.7 without deleting version 11.6?

install version11.7 when version11.6 is here

melanie_0-1691375946940.pngmelanie_1-1691376081714.png

Q2:my project is bulid by version11.7 .   could I use version 11.6 open it successfully?

0 Kudos
Reply
1 Reply

1,162 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi @melanie 

To Q1, I tried to reproduce, but no such issue as yours.

To Q2, In principle, it is not recommended to use it from the perspective of IDE, and the new options on the higher version may be lost in the lower version.

 

Best regards

Harvey

0 Kudos
Reply