adding ethernet controller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

adding ethernet controller

1,108 Views
ilanganor1
Contributor III

I am tryinh to add support for 2nd controlller as such, is it correct? is using fec is the correct way to go? are there missing things?:

+&fec {
+ pinctrl-names = "default";
+ pinctrl-0 = <&pinctrl_eqos1>;
+ phy-mode = "rgmii-id";
+ phy-handle = <&ethphy1>;
+ status = "okay";
+
+ mdio {
+ compatible = "snps,dwmac-mdio";
+ #address-cells = <1>;
+ #size-cells = <0>;
+
+ ethphy1: ethernet-phy@1 {
+ compatible = "brcm,bcm54616S";
+ reg = <1>;
+ };
+ };
+};
+
+
+
&flexspi {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_flexspi0>;
@@ -782,6 +804,24 @@
>;
};

+ pinctrl_eqos1: eqosgrp1 {
+ fsl,pins = <
+ MX8MP_IOMUXC_SD1_DATA2__ENET1_RGMII_RD0 0x91
+ MX8MP_IOMUXC_SD1_DATA3__ENET1_RGMII_RD1 0x91
+ MX8MP_IOMUXC_SAI1_RXD6__ENET1_RGMII_RD2 0x91
+ MX8MP_IOMUXC_SAI1_RXD7__ENET1_RGMII_RD3 0x91
+ MX8MP_IOMUXC_SAI1_TXFS__ENET1_RGMII_RX_CTL 0x91
+ MX8MP_IOMUXC_SAI1_TXC__ENET1_RGMII_RXC 0x91
+ MX8MP_IOMUXC_SD1_DATA1__ENET1_RGMII_TD0 0x1f
+ MX8MP_IOMUXC_SD1_DATA0__ENET1_RGMII_TD1 0x1f
+ MX8MP_IOMUXC_SAI1_TXD2__ENET1_RGMII_TD2 0x1f
+ MX8MP_IOMUXC_SAI1_TXD3__ENET1_RGMII_TD3 0x1f
+ MX8MP_IOMUXC_SAI1_TXD4__ENET1_RGMII_TX_CTL 0x1f
+ MX8MP_IOMUXC_SAI1_TXD5__ENET1_RGMII_TXC 0x1f
+ >;
+ };
+
+

0 Kudos
Reply
1 Reply

1,083 Views
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

Based on I.MX 8M Plus EVK device tree and 8M Plus reference manual, I would make this observations.

+&fec {
+ pinctrl-names = "default";
+ pinctrl-0 = <&pinctrl_eqos1>;
+ phy-mode = "rgmii-id";
+ phy-handle = <&ethphy1>;
+ status = "okay";
+
+ mdio {
+ #compatible = "snps,dwmac-mdio";
+ 
+ #address-cells = <1>;
+ #size-cells = <0>;
+
+ ethphy1: ethernet-phy@1 {
+ compatible = "brcm,bcm54616S";
+ reg = <1>;
+ };
+ };
+};
+
+
+
&flexspi {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_flexspi0>;
@@ -782,6 +804,24 @@
>;
};

+ pinctrl_eqos1: eqosgrp1 {
+ fsl,pins = <
+ MX8MP_IOMUXC_SAI1_RXD2__ENET1_MDC		0x2
+ MX8MP_IOMUXC_SAI1_RXD3__ENET1_MDIO		0x2
# 0x91 affects a reserved bit
+ MX8MP_IOMUXC_SD1_DATA2__ENET1_RGMII_RD0 0x90
+ MX8MP_IOMUXC_SD1_DATA3__ENET1_RGMII_RD1 0x90
+ MX8MP_IOMUXC_SAI1_RXD6__ENET1_RGMII_RD2 0x90
+ MX8MP_IOMUXC_SAI1_RXD7__ENET1_RGMII_RD3 0x90
+ MX8MP_IOMUXC_SAI1_TXFS__ENET1_RGMII_RX_CTL 0x90
+ MX8MP_IOMUXC_SAI1_TXC__ENET1_RGMII_RXC 0x90
# Alt mode 1
+ MX8MP_IOMUXC_SD1_DATA1__ENET1_RGMII_TD0 0x11
+ MX8MP_IOMUXC_SD1_DATA0__ENET1_RGMII_TD1 0x11
+ MX8MP_IOMUXC_SAI1_TXD2__ENET1_RGMII_TD2 0x11
+ MX8MP_IOMUXC_SAI1_TXD3__ENET1_RGMII_TD3 0x11
+ MX8MP_IOMUXC_SAI1_TXD4__ENET1_RGMII_TX_CTL 0x11
+ MX8MP_IOMUXC_SAI1_TXD5__ENET1_RGMII_TXC 0x11
+ >;
+ };
+
+

Regards

0 Kudos
Reply