adding ethernet controller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

adding ethernet controller

1,078件の閲覧回数
ilanganor1
Contributor III

I am tryinh to add support for 2nd controlller as such, is it correct? is using fec is the correct way to go? are there missing things?:

+&fec {
+ pinctrl-names = "default";
+ pinctrl-0 = <&pinctrl_eqos1>;
+ phy-mode = "rgmii-id";
+ phy-handle = <&ethphy1>;
+ status = "okay";
+
+ mdio {
+ compatible = "snps,dwmac-mdio";
+ #address-cells = <1>;
+ #size-cells = <0>;
+
+ ethphy1: ethernet-phy@1 {
+ compatible = "brcm,bcm54616S";
+ reg = <1>;
+ };
+ };
+};
+
+
+
&flexspi {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_flexspi0>;
@@ -782,6 +804,24 @@
>;
};

+ pinctrl_eqos1: eqosgrp1 {
+ fsl,pins = <
+ MX8MP_IOMUXC_SD1_DATA2__ENET1_RGMII_RD0 0x91
+ MX8MP_IOMUXC_SD1_DATA3__ENET1_RGMII_RD1 0x91
+ MX8MP_IOMUXC_SAI1_RXD6__ENET1_RGMII_RD2 0x91
+ MX8MP_IOMUXC_SAI1_RXD7__ENET1_RGMII_RD3 0x91
+ MX8MP_IOMUXC_SAI1_TXFS__ENET1_RGMII_RX_CTL 0x91
+ MX8MP_IOMUXC_SAI1_TXC__ENET1_RGMII_RXC 0x91
+ MX8MP_IOMUXC_SD1_DATA1__ENET1_RGMII_TD0 0x1f
+ MX8MP_IOMUXC_SD1_DATA0__ENET1_RGMII_TD1 0x1f
+ MX8MP_IOMUXC_SAI1_TXD2__ENET1_RGMII_TD2 0x1f
+ MX8MP_IOMUXC_SAI1_TXD3__ENET1_RGMII_TD3 0x1f
+ MX8MP_IOMUXC_SAI1_TXD4__ENET1_RGMII_TX_CTL 0x1f
+ MX8MP_IOMUXC_SAI1_TXD5__ENET1_RGMII_TXC 0x1f
+ >;
+ };
+
+

0 件の賞賛
返信
1 返信

1,053件の閲覧回数
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

Based on I.MX 8M Plus EVK device tree and 8M Plus reference manual, I would make this observations.

+&fec {
+ pinctrl-names = "default";
+ pinctrl-0 = <&pinctrl_eqos1>;
+ phy-mode = "rgmii-id";
+ phy-handle = <&ethphy1>;
+ status = "okay";
+
+ mdio {
+ #compatible = "snps,dwmac-mdio";
+ 
+ #address-cells = <1>;
+ #size-cells = <0>;
+
+ ethphy1: ethernet-phy@1 {
+ compatible = "brcm,bcm54616S";
+ reg = <1>;
+ };
+ };
+};
+
+
+
&flexspi {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_flexspi0>;
@@ -782,6 +804,24 @@
>;
};

+ pinctrl_eqos1: eqosgrp1 {
+ fsl,pins = <
+ MX8MP_IOMUXC_SAI1_RXD2__ENET1_MDC		0x2
+ MX8MP_IOMUXC_SAI1_RXD3__ENET1_MDIO		0x2
# 0x91 affects a reserved bit
+ MX8MP_IOMUXC_SD1_DATA2__ENET1_RGMII_RD0 0x90
+ MX8MP_IOMUXC_SD1_DATA3__ENET1_RGMII_RD1 0x90
+ MX8MP_IOMUXC_SAI1_RXD6__ENET1_RGMII_RD2 0x90
+ MX8MP_IOMUXC_SAI1_RXD7__ENET1_RGMII_RD3 0x90
+ MX8MP_IOMUXC_SAI1_TXFS__ENET1_RGMII_RX_CTL 0x90
+ MX8MP_IOMUXC_SAI1_TXC__ENET1_RGMII_RXC 0x90
# Alt mode 1
+ MX8MP_IOMUXC_SD1_DATA1__ENET1_RGMII_TD0 0x11
+ MX8MP_IOMUXC_SD1_DATA0__ENET1_RGMII_TD1 0x11
+ MX8MP_IOMUXC_SAI1_TXD2__ENET1_RGMII_TD2 0x11
+ MX8MP_IOMUXC_SAI1_TXD3__ENET1_RGMII_TD3 0x11
+ MX8MP_IOMUXC_SAI1_TXD4__ENET1_RGMII_TX_CTL 0x11
+ MX8MP_IOMUXC_SAI1_TXD5__ENET1_RGMII_TXC 0x11
+ >;
+ };
+
+

Regards

0 件の賞賛
返信