adding LTE modem via UART [iMX7Dual]

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

adding LTE modem via UART [iMX7Dual]

1,096 Views
mrlantz
Contributor I

I need to configure IMX7D to support LTE modem via UART interface. Anyone done this or is it already supported and only need to reconfigure from default PCIe (I guess that this are default if your red the specification) to UART?

Labels (3)
0 Kudos
Reply
1 Reply

1,000 Views
igorpadykov
NXP Employee
NXP Employee

Hi johan

usually modem porting guidelines are provided by
modem vendor and it may be specific for every modem model,
recommended to apply to support of that modem for porting
examples.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply