adding LTE modem via UART [iMX7Dual]

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

adding LTE modem via UART [iMX7Dual]

1,504 次查看
mrlantz
Contributor I

I need to configure IMX7D to support LTE modem via UART interface. Anyone done this or is it already supported and only need to reconfigure from default PCIe (I guess that this are default if your red the specification) to UART?

标签 (3)
0 项奖励
回复
1 回复

1,408 次查看
igorpadykov
NXP Employee
NXP Employee

Hi johan

usually modem porting guidelines are provided by
modem vendor and it may be specific for every modem model,
recommended to apply to support of that modem for porting
examples.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复