add file to boot partition of sdcard image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

add file to boot partition of sdcard image

1,932 Views
rob_lepage
Contributor I

I am putting together an sdcard image to boot an imx.6ull and automatically program on board nand flash.  I am able to generate an sdcard image that boots and ubifs rootfs.  I have also increase the boot partition size in the sdcard image to make space for a copy of the ubifs.

My question is how can I have yocto automatically include the ubifs rootfs in the boot partition of the sdcard image?

Thanks for any help offered.

Labels (2)
0 Kudos
Reply
1 Reply

1,792 Views
b36401
NXP Employee
NXP Employee

You can refer to these yocto documents regarding to adding features:

https://community.nxp.com/docs/DOC-1616
https://community.nxp.com/docs/DOC-95333

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply