about Internal POR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

about Internal POR

Jump to solution
1,963 Views
goto11
Contributor III

Hello,Community

I was able to find a description of the state where the reset was released.
Please tell me the VDD_ARM voltage and VDD_SOC voltage that is reset or reset is released.

Excerpt from section 6.2.5 of i.MX 7Dual Applications Processor Reference Manual

• 4ms after the external power supply VDDHIGH_IN is valid
• 1ms after the VDD_SOC_CAP supply is valid

best regards

Goto

Labels (1)
0 Kudos
Reply
1 Solution
1,900 Views
Yuri
NXP Employee
NXP Employee

Hello,

   Table 9 (Operating ranges) of the Datasheet(s) may be used for minimal allowed voltage

values:

VDD_ARM   - 0.95 V

VDD_SOC  - 0.95 V

https://www.nxp.com/docs/en/data-sheet/IMX7DCEC.pdf 

Regards,

Yuri.

View solution in original post

0 Kudos
Reply
1 Reply
1,901 Views
Yuri
NXP Employee
NXP Employee

Hello,

   Table 9 (Operating ranges) of the Datasheet(s) may be used for minimal allowed voltage

values:

VDD_ARM   - 0.95 V

VDD_SOC  - 0.95 V

https://www.nxp.com/docs/en/data-sheet/IMX7DCEC.pdf 

Regards,

Yuri.

0 Kudos
Reply