about GPIO DC Parameters

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

about GPIO DC Parameters

1,287件の閲覧回数
goto11
Contributor III

Hello,Community

About i.MX 7Dual Family of Applications Processors Datasheet Table 29. GPIO DC Parameters
The Min value and Max value of the following parameter are defined by the following formula.
High-level output voltage (VOH) Min is 0.8 × OVDD
Low-level output voltage (VOL) Max is 0.2 × OVDD
Test Conditions are IOH = –1.8mA, –3.6mA, –7.2mA, –10.8mA, IOL = 1.8mA, 3.6mA, 7.2mA, 10.8mA.


In reality, it does not carry that much current.
Please tell me VOH (min) and VOL (max) when the current is lower.
Or if I have a current versus voltage graph, I want.

For example, when VOH and VIL conditions of Table 22. GPIO DC Parameters of i.MX 6Solo / 6DualLite Applications Processors for Industrial Products

Best Reguards

Goto

ラベル(1)
0 件の賞賛
返信
1 返信

1,241件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

   Use i.MX7 IBIS model in order to get current versus voltage curve.

 

https://www.nxp.com/webapp/Download?colCode=IMX7D_IBIS 

https://community.nxp.com/message/381665 

Have a great day,

Yuri

 

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 件の賞賛
返信