about EIM timing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

about EIM timing

Jump to solution
2,290 Views
george
Senior Contributor II

Dear all,

We have planned the product using i.MX6Solo.

The product runs by original RTOS.

For the reason, we are reading the documents in detail.

Please let me know about the timing of EIM.

About the description of page 58 into the data sheet(http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf)

pastedImage_1.png

Best Regards,

George

Labels (3)
Tags (5)
1 Solution
2,071 Views
igorpadykov
NXP Employee
NXP Employee

Hi George

regarding upper arrow: yes, correct reading is "WE41A"

low arrow: "WE42" - this is misprint, can be ignored.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,072 Views
igorpadykov
NXP Employee
NXP Employee

Hi George

regarding upper arrow: yes, correct reading is "WE41A"

low arrow: "WE42" - this is misprint, can be ignored.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,071 Views
george
Senior Contributor II

Thanks

BR

0 Kudos
Reply