about EIM timing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,289件の閲覧回数
george
Senior Contributor II

Dear all,

We have planned the product using i.MX6Solo.

The product runs by original RTOS.

For the reason, we are reading the documents in detail.

Please let me know about the timing of EIM.

About the description of page 58 into the data sheet(http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf)

pastedImage_1.png

Best Regards,

George

ラベル(3)
タグ(5)
1 解決策
2,070件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi George

regarding upper arrow: yes, correct reading is "WE41A"

low arrow: "WE42" - this is misprint, can be ignored.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,071件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi George

regarding upper arrow: yes, correct reading is "WE41A"

low arrow: "WE42" - this is misprint, can be ignored.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,070件の閲覧回数
george
Senior Contributor II

Thanks

BR

0 件の賞賛
返信