a problem about i.MX53

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

a problem about i.MX53

ソリューションへジャンプ
3,680件の閲覧回数
chunlinchen
Contributor I

hi,I custom a board ,the processer is  i.MX537, the design is very similar with i.MX 535QSB.

when i test usb ,the windows display “Unknow device”,I check  the power supply and all  voltage  are OK.

Anybody has  experience about this?

Best Regards!

タグ(1)
0 件の賞賛
返信
1 解決策
3,508件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please try using an external self-powered USB hub between i.MX53 and PC.

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
3,508件の閲覧回数
Yuri
NXP Employee
NXP Employee

Do You mean USB issue with internal UART / USB boot(ROM)loader of the i.MX53 or problems with OS (Linux) under i.MX53 ?

0 件の賞賛
返信
3,508件の閲覧回数
chunlinchen
Contributor I

The driver is ok.now my problem is that the windows can not identify  theUSB device,display “unknown device”.

I checked the USB part of our design,no mistake was found.

0 件の賞賛
返信
3,509件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please try using an external self-powered USB hub between i.MX53 and PC.

0 件の賞賛
返信
3,507件の閲覧回数
chunlinchen
Contributor I

Hi:

   Thanks for your suggestion,this problem was solved.

   Best Regards !

0 件の賞賛
返信
3,507件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

It could probably be that you don't have an HID driver installed on your PC.

0 件の賞賛
返信
3,508件の閲覧回数
chunlinchen
Contributor I

I use the MFGTool,and I installed the driver.when i use the i.MX53QSB,and work well,so I think the driver is ok?

0 件の賞賛
返信