a problem about i.MX53

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

a problem about i.MX53

跳至解决方案
3,606 次查看
chunlinchen
Contributor I

hi,I custom a board ,the processer is  i.MX537, the design is very similar with i.MX 535QSB.

when i test usb ,the windows display “Unknow device”,I check  the power supply and all  voltage  are OK.

Anybody has  experience about this?

Best Regards!

标记 (1)
0 项奖励
回复
1 解答
3,434 次查看
Yuri
NXP Employee
NXP Employee

Please try using an external self-powered USB hub between i.MX53 and PC.

在原帖中查看解决方案

0 项奖励
回复
6 回复数
3,434 次查看
Yuri
NXP Employee
NXP Employee

Do You mean USB issue with internal UART / USB boot(ROM)loader of the i.MX53 or problems with OS (Linux) under i.MX53 ?

0 项奖励
回复
3,434 次查看
chunlinchen
Contributor I

The driver is ok.now my problem is that the windows can not identify  theUSB device,display “unknown device”.

I checked the USB part of our design,no mistake was found.

0 项奖励
回复
3,435 次查看
Yuri
NXP Employee
NXP Employee

Please try using an external self-powered USB hub between i.MX53 and PC.

0 项奖励
回复
3,433 次查看
chunlinchen
Contributor I

Hi:

   Thanks for your suggestion,this problem was solved.

   Best Regards !

0 项奖励
回复
3,433 次查看
SergioSolis
NXP Employee
NXP Employee

It could probably be that you don't have an HID driver installed on your PC.

0 项奖励
回复
3,434 次查看
chunlinchen
Contributor I

I use the MFGTool,and I installed the driver.when i use the i.MX53QSB,and work well,so I think the driver is ok?

0 项奖励
回复