a problem about i.MX53

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

a problem about i.MX53

Jump to solution
3,678 Views
chunlinchen
Contributor I

hi,I custom a board ,the processer is  i.MX537, the design is very similar with i.MX 535QSB.

when i test usb ,the windows display “Unknow device”,I check  the power supply and all  voltage  are OK.

Anybody has  experience about this?

Best Regards!

Tags (1)
0 Kudos
Reply
1 Solution
3,506 Views
Yuri
NXP Employee
NXP Employee

Please try using an external self-powered USB hub between i.MX53 and PC.

View solution in original post

0 Kudos
Reply
6 Replies
3,506 Views
Yuri
NXP Employee
NXP Employee

Do You mean USB issue with internal UART / USB boot(ROM)loader of the i.MX53 or problems with OS (Linux) under i.MX53 ?

0 Kudos
Reply
3,506 Views
chunlinchen
Contributor I

The driver is ok.now my problem is that the windows can not identify  theUSB device,display “unknown device”.

I checked the USB part of our design,no mistake was found.

0 Kudos
Reply
3,507 Views
Yuri
NXP Employee
NXP Employee

Please try using an external self-powered USB hub between i.MX53 and PC.

0 Kudos
Reply
3,505 Views
chunlinchen
Contributor I

Hi:

   Thanks for your suggestion,this problem was solved.

   Best Regards !

0 Kudos
Reply
3,505 Views
SergioSolis
NXP Employee
NXP Employee

It could probably be that you don't have an HID driver installed on your PC.

0 Kudos
Reply
3,506 Views
chunlinchen
Contributor I

I use the MFGTool,and I installed the driver.when i use the i.MX53QSB,and work well,so I think the driver is ok?

0 Kudos
Reply