Yocto project source scm-imx-3.14.52-1.1.0_ga not available

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Yocto project source scm-imx-3.14.52-1.1.0_ga not available

Jump to solution
2,220 Views
disheng
Contributor III

Hello,

I am trying to download Yocto project source for  scm-imx-3.14.52-1.1.0_ga with:

repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b scm-imx-3.14.52-1.1.0_ga

but it seems no longer available and I was trying with:

repo init -u https://source.codeaurora.org/external/imx/fsl-arm-yocto-bsp -b scm-imx-3.14.52-1.1.0_ga

also no luck.

Could you point to the location where I can download this?

 

Thank you.

0 Kudos
Reply
1 Solution
2,213 Views
nxf63675
NXP TechSupport
NXP TechSupport

Hi disheng,

 

You can find the info here:

https://source.codeaurora.org/external/imx/fsl-arm-yocto-bsp/commit/?h=imx-3.14.52-1.1.0_ga

 

This a very old distribution, I recommend you to update a new one, you can find all the distribution that we have here:

https://www.nxp.com/design/software/embedded-software/i-mx-software:IMX-SW

 

Hope this helps you.

Regards,

Israel.

View solution in original post

0 Kudos
Reply
4 Replies
2,214 Views
nxf63675
NXP TechSupport
NXP TechSupport

Hi disheng,

 

You can find the info here:

https://source.codeaurora.org/external/imx/fsl-arm-yocto-bsp/commit/?h=imx-3.14.52-1.1.0_ga

 

This a very old distribution, I recommend you to update a new one, you can find all the distribution that we have here:

https://www.nxp.com/design/software/embedded-software/i-mx-software:IMX-SW

 

Hope this helps you.

Regards,

Israel.

0 Kudos
Reply
2,204 Views
disheng
Contributor III

Hi Israel,

Thanks for the reply.

We are replacing the ddr on our custom board which referred to the imx6DL scm board with Android 5.1 and I only wanted the yocto source code to rebuild the MFG tool Firmware, that is why I want that particular release, since the source code you mentioned does not have the configuration for the SCM board.

 

Thank you,

Di

0 Kudos
Reply
2,198 Views
nxf63675
NXP TechSupport
NXP TechSupport

Hi disheng,

 

I see and understand your problem, It is unfortunately to say that we do not support that version of android any more, and that's why you can't find It on the official web page.

Sorry for the problems that this may cause you.

 

Regads,

Israel.

0 Kudos
Reply
2,194 Views
disheng
Contributor III

Hi Israel,

Ok, thanks.

Somehow it seems there is a meta-fsl-scm.tar.gz file which I can use under the fsl-arm-yocto-bsp according this this thread:

https://community.nxp.com/t5/i-MX-Processors/SCM-i-MX-6Dual-6Quad-Linux-Patch-not-able-to-bitbake/m-...

And there is also a document SCMIMX6DQLRNUG but I could not find anywhere.

Could you provide the meta-fsl-scm.tar.gz and SCMIMX6DQLRNUG if possible? Thank you very much!

 

Regards,

Di

0 Kudos
Reply