Yocto project host setup

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Yocto project host setup

2,921 次查看
hailiu
Contributor IV

Dear friends ,

I am setting up a host for L5.4... yocto project. Based on the document, I should install package python, pylint3 and rsnc. When I install them, the installer say install pynthon-is-pynth2, git, and pylint should be installed instead of these specified in document . It also say that the package Rsnc can not be located. Is rsnc a typo?  Is rsnc should be rsync instead?

 

thank you

Hai

0 项奖励
回复
4 回复数

2,914 次查看
hailiu
Contributor IV

ubuntu 20.04, when I use 20.04, It seems the repo sync has problem. i t give me error like this:

curl: (28) Failed to connect to github.com port 443: Connection timed ou

should I use 18.04?

0 项奖励
回复

2,910 次查看
hailiu
Contributor IV

Dear joan

Switched to 18.04, rsnc still can not be found。I tried to do the repo sync, errors occured. Attanched is a sanpshot.

the following is the error message.

fatal: unable to access 'https://github.com/meta-rust/meta-rust/': Failed to connect to github.com port 443: Connection timed out

 

thank you

Hai

0 项奖励
回复

2,896 次查看
joanxie
NXP TechSupport
NXP TechSupport

this is your network connection issue, you need check your network and try again, before you building, don't forget install all of packages in the chapter 3 Host Setup and chapter 1.2.1. Ubuntu and Debian of

"https://www.yoctoproject.org/docs/3.0/ref-manual/ref-manual.html#ubuntu-packages"

if you forget install something, I suggest that you delete the build folder, install first, then build again

 

0 项奖励
回复

2,915 次查看
joanxie
NXP TechSupport
NXP TechSupport

what ubuntu version do you use? ubuntu 18.04? and send the message or screen shot to me, let me check the detailed information when you install them

0 项奖励
回复