Yocto iMX8M Plus boot kernel loop with "eth_lpi not found"

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Yocto iMX8M Plus boot kernel loop with "eth_lpi not found"

跳至解决方案
2,894 次查看
cygnus
Contributor I

iMX8M Plus configured for Yocto on Variscite DART-MX8M-PLUS, booting from eMMC.

While starting the kernel it fails to ever finish booting as it loops, printing "IRQ eth_lpi not found" messages over and over. I suspect the issue might be with the device tree but do not know for certain and also do not know how this would be remedied.

Boot log is attached.

Thank you in advance for any guidance.

0 项奖励
回复
1 解答
2,875 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

It could be problem with the connection, but maybe some @variscite could help.

regards

在原帖中查看解决方案

0 项奖励
回复
5 回复数
1,955 次查看
rkettridge
Contributor I
Sorry to pull up an old thread, but did you get a resolution to this? We're in exactly the same situation with exactly the same error messages. We are in touch with Variscite but if you have a quick solution, or even just a pointer, we might get there quicker.
0 项奖励
回复
1,949 次查看
cygnus
Contributor I

Hi, sorry to leave the post unanswered. I did resolve the issue;

Variscite responded to me with the following after I described the issue to them:

"The message you are reporting is just an expected harmless warning.
You may want to edit the device tree and remove the second ethernet here
https://github.com/varigit/linux-imx/blob/lf-6.1.y_var03/arch/arm64/boot/dts/freescale/imx8mp-var-da..."

Upon removing the &eqos and &fec blocks from the device tree, the warning message disappeared. Not sure why this seems to have prevented it from booting.

Hopefully this helps.

0 项奖励
回复
1,938 次查看
rkettridge
Contributor I
Thanks for the quick reply. In our case we do have both Ethernet devices but one is not being seen. As you say, it’s odd it stops it booting. Shall continue discussions with Variscite support.

Thanks again. The device tree link may come in handy.
0 项奖励
回复
2,856 次查看
eranmatityahu
Contributor IV

Hi @cygnus.

If you are a Variscite customer, please register and create a ticket in the Variscite customer portal, and provide more details about the carrier board you are using: https://varisciteportal.axosoft.com/

 

Thanks,
Eran

0 项奖励
回复
2,876 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

It could be problem with the connection, but maybe some @variscite could help.

regards

0 项奖励
回复