I attempted to write a program to just do a hash-2 512. This results in the smw_hash() function calling exit(1). We also would like to do AES 256 with this library which will require key generation and storage.
Are there any example programs I could look at? I realize there is a test program, which does work, but it is much more complicated than what I would like to do.
Here is a trace of what I see, just calling smw_hash:
#0 __GI__exit (status=status@entry=1) at /usr/src/debug/glibc/2.39+git/sysdeps/unix/sysv/linux/_exit.c:27
#1 0x0000fffff7d8e0e0 in __run_exit_handlers (status=status@entry=1, listp=0xfffff7ef0660 <__exit_funcs>, run_list_atexit=run_list_atexit@entry=true, run_dtors=run_dtors@entry=true) at exit.c:131
#2 0x0000fffff7d8e1f0 in __GI_exit (status=status@entry=1) at exit.c:138
#3 0x0000fffff7f90e88 in config_db_mutex_lock () at /usr/src/debug/smw/git/core/config/database.c:66
#4 0x0000fffff7f916fc in smw_config_select_subsystem (operation_id=OPERATION_ID_HASH, args=0xfffffffff958, subsystem_id=subsystem_id@entry=0xfffffffff94c) at /usr/src/debug/smw/git/core/config/database.c:560
#5 0x0000fffff7f7beb8 in smw_utils_execute_common (operation_id=operation_id@entry=OPERATION_ID_HASH, args=args@entry=0xfffffffff958, subsystem_id=<optimized out>, op_step=op_step@entry=SMW_OP_STEP_ONESHOT,
implicit=implicit@entry=false) at /usr/src/debug/smw/git/core/utils/exec.c:38
#6 0x0000fffff7f7bf04 in smw_utils_execute_operation (operation_id=operation_id@entry=OPERATION_ID_HASH, args=args@entry=0xfffffffff958, subsystem_id=<optimized out>)
at /usr/src/debug/smw/git/core/utils/exec.c:89
#7 0x0000fffff7f88728 in smw_hash (args=args@entry=0xfffffffff9b8) at /usr/src/debug/smw/git/core/crypto/hash.c:115
#8 0x0000aaaaaaaa0a84 in main () at simplehash.c:38
This appears to be the cause of the EXIT:
SMW_DBG_ASSERT(ctx);
In my code, I did this prior to calling smw_hash, and it is not getting an error:
memset(&ctx_args, 0, sizeof(ctx_args));
ctx_args.subsystem_name = SMW_SUBSYSTEM_NAME_ELE;
// Allocate context
smw_result = smw_allocate_context(&ctx_args);
if (smw_result != SMW_STATUS_OK) {
printf("Failed to allocate context: %d\n", smw_result);
return -1;
}
I am using IMX91 with FRDM board, and am building with imx-6.6.36-2.1.0.xml.