Yocto iMX Camera and Player QT apps no preview content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Yocto iMX Camera and Player QT apps no preview content

1,668 Views
mayqueen
Contributor IV

Hello All:

Platform: i.MX6

OS: Yocto Morty

Kernel: 4.9.11

Display: HDMI 720P

As title, I think it's old problems since I touch Yocto with 4.1.15 kernel, How to fix no preview content in iMX Camera and iMX Player apps? It works if I issue Gstreammer commands, but no display for QT apps.

Thanks

Wig

Labels (3)
0 Kudos
Reply
2 Replies

1,393 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Wig,

Would you please give us a bit more information? Are you using the 4.9 BSP Release or the morty branch from the Community BSP directly? Are you using X11 as distro?

Did you have these problems also on BSP Release 4.1.15?

Regards,

1,393 Views
mayqueen
Contributor IV

Hello! It works already when I modify imx6q-pistachio.dts (my board) and enable mxcfb1 to mxcfb4..
And another trick is the boot argument have to take out "bpp=32" setting...

I think it's due to the FSL apps has some hard code to detect demo board setting but I'm not trace yet, after all,  I know what's going on, thanks!

0 Kudos
Reply