Yocto iMX Camera and Player QT apps no preview content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Yocto iMX Camera and Player QT apps no preview content

1,660件の閲覧回数
mayqueen
Contributor IV

Hello All:

Platform: i.MX6

OS: Yocto Morty

Kernel: 4.9.11

Display: HDMI 720P

As title, I think it's old problems since I touch Yocto with 4.1.15 kernel, How to fix no preview content in iMX Camera and iMX Player apps? It works if I issue Gstreammer commands, but no display for QT apps.

Thanks

Wig

ラベル(3)
タグ(4)
0 件の賞賛
返信
2 返答(返信)

1,385件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Wig,

Would you please give us a bit more information? Are you using the 4.9 BSP Release or the morty branch from the Community BSP directly? Are you using X11 as distro?

Did you have these problems also on BSP Release 4.1.15?

Regards,

1,385件の閲覧回数
mayqueen
Contributor IV

Hello! It works already when I modify imx6q-pistachio.dts (my board) and enable mxcfb1 to mxcfb4..
And another trick is the boot argument have to take out "bpp=32" setting...

I think it's due to the FSL apps has some hard code to detect demo board setting but I'm not trace yet, after all,  I know what's going on, thanks!

0 件の賞賛
返信