Yocto iMX Camera and Player QT apps no preview content

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Yocto iMX Camera and Player QT apps no preview content

1,661 次查看
mayqueen
Contributor IV

Hello All:

Platform: i.MX6

OS: Yocto Morty

Kernel: 4.9.11

Display: HDMI 720P

As title, I think it's old problems since I touch Yocto with 4.1.15 kernel, How to fix no preview content in iMX Camera and iMX Player apps? It works if I issue Gstreammer commands, but no display for QT apps.

Thanks

Wig

标签 (3)
标记 (4)
0 项奖励
回复
2 回复数

1,386 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Wig,

Would you please give us a bit more information? Are you using the 4.9 BSP Release or the morty branch from the Community BSP directly? Are you using X11 as distro?

Did you have these problems also on BSP Release 4.1.15?

Regards,

1,386 次查看
mayqueen
Contributor IV

Hello! It works already when I modify imx6q-pistachio.dts (my board) and enable mxcfb1 to mxcfb4..
And another trick is the boot argument have to take out "bpp=32" setting...

I think it's due to the FSL apps has some hard code to detect demo board setting but I'm not trace yet, after all,  I know what's going on, thanks!

0 项奖励
回复