Yocto for iMX8MP if giving fetch error.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Yocto for iMX8MP if giving fetch error.

ソリューションへジャンプ
6,317件の閲覧回数
shravankumaralugala
Contributor II

The sourceaurora repository(for iMX8MP) is now working , due to which I are not able to generate the binaries.

Can any one help to resolve this issue.

 

Below is error log: 

ERROR: u-boot-imx-tools-native-2022.04-r0 do_fetch: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; export DBUS_SESSION_BUS_ADDRESS="unix:path=/run/user/1000/bus"; export SSH_AUTH_SOCK="/run/user/1000/keyring/ssh"; export PATH="/home/cmd/u01/es_yocto_master_merge/es-yocto-configuration/yocto-layers/poky/scripts/native-intercept:/home/cmd/u01/es_yocto_master_merge/es-yocto-configuration/build/tmp/sysroots-uninative/x86_64-linux/usr/bin:/home/cmd/u01/es_yocto_master_merge/es-yocto-configuration/yocto-layers/poky/scripts:/home/cmd/u01/es_yocto_master_merge/es-yocto-configuration/build/tmp/work/x86_64-linux/u-boot-imx-tools-native/2022.04-r0/recipe-sysroot-native/usr/bin/x86_64-linux:/home/cmd/u01/es_yocto_master_merge/es-yocto-configuration/build/tmp/work/x86_64-linux/u-boot-imx-tools-native/2022.04-r0/recipe-sysroot-native/usr/bin:/home/cmd/u01/es_yocto_master_merge/es-yocto-configuration/build/tmp/work/x86_64-linux/u-boot-imx-tools-native/2022.04-r0/recipe-sysroot-native/usr/sbin:/home/cmd/u01/es_yocto_master_merge/es-yocto-configuration/build/tmp/work/x86_64-linux/u-boot-imx-tools-native/2022.04-r0/recipe-sysroot-native/usr/bin:/home/cmd/u01/es_yocto_master_merge/es-yocto-configuration/build/tmp/work/x86_64-linux/u-boot-imx-tools-native/2022.04-r0/recipe-sysroot-native/sbin:/home/cmd/u01/es_yocto_master_merge/es-yocto-configuration/build/tmp/work/x86_64-linux/u-boot-imx-tools-native/2022.04-r0/recipe-sysroot-native/bin:/home/cmd/u01/es_yocto_master_merge/es-yocto-configuration/yocto-layers/poky/bitbake/bin:/home/cmd/u01/es_yocto_master_merge/es-yocto-configuration/build/tmp/hosttools"; export HOME="/home/cmd"; LANG=C git -c core.fsyncobjectfiles=0 -c gc.autoDetach=false -c core.pager=cat clone --bare --mirror https://source.codeaurora.org/external/imx/uboot-imx.git /home/cmd/u01/es_yocto_master_merge/es-yocto-configuration/build/downloads/git2/source.codeaurora.org.external.imx.uboot-imx.git --progress failed with exit code 128, no output

ERROR: u-boot-imx-tools-native-2022.04-r0 do_fetch: Bitbake Fetcher Error: FetchError('Unable to fetch URL from any source.', 'git://source.codeaurora.org/external/imx/uboot-imx.git;protocol=https;branch=lf_v2022.04')

ERROR: Logfile of failure stored in: /home/cmd/u01/es_yocto_master_merge/es-yocto-configuration/build/tmp/work/x86_64-linux/u-boot-imx-tools-native/2022.04-r0/temp/log.do_fetch.538226

ERROR: Task (virtual:native:/home/cmd/u01/es_yocto_master_merge/es-yocto-configuration/build/../yocto-layers/meta-imx/meta-bsp/recipes-bsp/u-boot/u-boot-imx-tools_2022.04.bb:do_fetch) failed with exit code '1'

ラベル(1)
0 件の賞賛
返信
1 解決策
6,305件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

the Linux BSP from CodeAurora to Github, the app team is still work on it, try to change the repo command to repo init -u https://github.com/nxp-imx/imx-manifest -b <branch name> [ -m <release manifest>]

元の投稿で解決策を見る

5 返答(返信)
6,306件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

the Linux BSP from CodeAurora to Github, the app team is still work on it, try to change the repo command to repo init -u https://github.com/nxp-imx/imx-manifest -b <branch name> [ -m <release manifest>]

5,155件の閲覧回数
dkprashant
Contributor II

Hi,

I am still facing this error. I am trying to download imx8-kirkstone-5.15 kernel. But the kernel fetch always fails. I have tried in multiple systems with good network connections. Below are the steps followed

 

$: repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-kirkstone -m imx-5.15.52-2.1.0.xml

$ repo sync

$ MACHINE=imx8mpevk DISTRO=fsl-imx-xwayland source ./imx-setup-release.sh -b bld-xwayland

$  bitbake imx-image-full

 

ERROR: linux-imx-5.15.52+gitAUTOINC+36363d8623-r0 do_fetch: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; export DBUS_SESSION_BUS_ADDRESS="unix:path=/run/user/1000/bus"; export PATH="/home/ametek/pkulkarni/imx8_rel/bld-xwayland/tmp/sysroots-uninative/x86_64-linux/usr/bin:/home/ametek/pkulkarni/imx8_rel/sources/poky/scripts:/home/ametek/pkulkarni/imx8_rel/bld-xwayland/tmp/work/imx8mpevk-poky-linux/linux-imx/5.15.52+gitAUTOINC+36363d8623-r0/recipe-sysroot-native/usr/bin/aarch64-poky-linux:/home/ametek/pkulkarni/imx8_rel/bld-xwayland/tmp/work/imx8mpevk-poky-linux/linux-imx/5.15.52+gitAUTOINC+36363d8623-r0/recipe-sysroot/usr/bin/crossscripts:/home/ametek/pkulkarni/imx8_rel/bld-xwayland/tmp/work/imx8mpevk-poky-linux/linux-imx/5.15.52+gitAUTOINC+36363d8623-r0/recipe-sysroot-native/usr/sbin:/home/ametek/pkulkarni/imx8_rel/bld-xwayland/tmp/work/imx8mpevk-poky-linux/linux-imx/5.15.52+gitAUTOINC+36363d8623-r0/recipe-sysroot-native/usr/bin:/home/ametek/pkulkarni/imx8_rel/bld-xwayland/tmp/work/imx8mpevk-poky-linux/linux-imx/5.15.52+gitAUTOINC+36363d8623-r0/recipe-sysroot-native/sbin:/home/ametek/pkulkarni/imx8_rel/bld-xwayland/tmp/work/imx8mpevk-poky-linux/linux-imx/5.15.52+gitAUTOINC+36363d8623-r0/recipe-sysroot-native/bin:/home/ametek/pkulkarni/imx8_rel/sources/poky/bitbake/bin:/home/ametek/pkulkarni/imx8_rel/bld-xwayland/tmp/hosttools"; export HOME="/home/ametek"; LANG=C git -c core.fsyncobjectfiles=0 -c gc.autoDetach=false -c core.pager=cat clone --bare --mirror https://github.com/nxp-imx/linux-imx.git /home/ametek/pkulkarni/imx8_rel/downloads//git2/github.com.nxp-imx.linux-imx.git --progress failed with exit code 128, no output
ERROR: linux-imx-5.15.52+gitAUTOINC+36363d8623-r0 do_fetch: Bitbake Fetcher Error: FetchError('Unable to fetch URL from any source.', 'git://github.com/nxp-imx/linux-imx.git;protocol=https;branch=lf-5.15.y')

0 件の賞賛
返信
5,086件の閲覧回数
dkprashant
Contributor II

The problem got resolved after re-installing certificates.

sudo apt install --reinstall ca-certificates

 

1,489件の閲覧回数
AlekseyM
Contributor III
Worked for me
0 件の賞賛
返信
5,055件の閲覧回数
davisroman3
Contributor III

Worked for me as well. Thanks!

0 件の賞賛
返信