Yocto build error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Yocto build error

5,272件の閲覧回数
bharadwaaj
Contributor III

Hi tried to compile Linux for sambrae dual light auto... got this error google search yielded me nothing. Need help to rectify it...

DEBUG: Executing python function do_unpack
DEBUG: Executing python function base_do_unpack
NOTE: Unpacking /home/sudoer/fsl-release-bsp-x11/downloads/hicolor-icon-theme-0.12.tar.gz to /home/sudoer/fsl-release-bsp-x11/build/tmp/work/all-poky-linux/hicolor-icon-theme/0.12-r1/

gzip: stdin: unexpected end of file
tar: Child returned status 1
tar: Error is not recoverable: exiting now
DEBUG: Python function base_do_unpack finished
DEBUG: Python function do_unpack finished
ERROR: Function failed: Unpack failure for URL: 'http://icon-theme.freedesktop.org/releases/hicolor-icon-theme-0.12.tar.gz'. Unpack command PATH="/home/sudoer/fsl-release-bsp-x11/sources/poky/scripts:/home/sudoer/fsl-release-bsp-x11/build/tmp/sysroots/x86_64-linux/usr/bin/cortexa9hf-vfp-neon-poky-linux:/home/sudoer/fsl-release-bsp-x11/build/tmp/sysroots/imx6dlsabreauto/usr/bin/crossscripts:/home/sudoer/fsl-release-bsp-x11/build/tmp/sysroots/x86_64-linux/usr/sbin:/home/sudoer/fsl-release-bsp-x11/build/tmp/sysroots/x86_64-linux/usr/bin:/home/sudoer/fsl-release-bsp-x11/build/tmp/sysroots/x86_64-linux/sbin:/home/sudoer/fsl-release-bsp-x11/build/tmp/sysroots/x86_64-linux//bin:/home/sudoer/fsl-release-bsp-x11/sources/poky/scripts:/home/sudoer/fsl-release-bsp-x11/sources/poky/bitbake/bin:/home/sudoer/bin:/home/sudoer/bin:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games:/usr/local/games" tar xz --no-same-owner -f /home/sudoer/fsl-release-bsp-x11/downloads/hicolor-icon-theme-0.12.tar.gz failed with return value 2
~                           

タグ(3)
0 件の賞賛
返信
1 返信

3,063件の閲覧回数
saurabh206
Senior Contributor III

Hi,

you can download "http://icon-theme.freedesktop.org/releases/hicolor-icon-theme-0.12.tar.gz.' manually and copied it to your download folder.

Create hicolor-icon-theme-0.12.tar.gz.done file in download folder.

Build again. It should fixed your issue.

Thanks

Saurabh

0 件の賞賛
返信