Yocto Task #1 - Download the source code ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Yocto Task #1 - Download the source code ?

跳至解决方案
3,378 次查看
anaseem
Contributor IV

To create embedded Linux image for imx8qxpmek evaluation board, I went to Yocto Training - Home as follows:

I started with Task #1 - Download the source code.  I was expecting that Task #1 would contain command to Download poky source:  $ git clone git://git.yoctoproject.org/poky --branch warrior

And then I thought Task #1 would provide following command to prepare the build:

$ source oe-init-build-en <build_directory>

But Task #1 is providing commands to download BSP source.  For which board are we downloading the BSP source?

Why is Task #1 asking to Download source code from community and NXP Code Aurora?  Shouldn't it be one or the other?

Do I need to Download poky source code using the git command above?  Or I'll get every needed to build yocto using commands in Task #1 ?

标记 (1)
1 解答
3,148 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Amer Naseem,


The Yocto training you are referencing to is focused on the Community BSP (more information on the link below)
https://freescale.github.io/#documentation


If you are working with an NXP board I would recommend starting with one of the BSP Releases, available at the following link:
https://www.nxp.com/design/software/embedded-software/linux-software-and-development-tools/embedded-...


For the imx8qxpmek board the latest BSP Release available is L4.19.35_1.1.0. You can download the documentation for this BSP on the link below (you may need to login to download this documentation bundle)

https://www.nxp.com/webapp/Download?colCode=L4.19.35_1.1.0_LINUX_DOCS


Inside, you will find the i.MX Yocto Project User's Guide, which has instructions on how to setup Yocto on your host machine to build images for this board.


Regards,

在原帖中查看解决方案

1 回复
3,149 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Amer Naseem,


The Yocto training you are referencing to is focused on the Community BSP (more information on the link below)
https://freescale.github.io/#documentation


If you are working with an NXP board I would recommend starting with one of the BSP Releases, available at the following link:
https://www.nxp.com/design/software/embedded-software/linux-software-and-development-tools/embedded-...


For the imx8qxpmek board the latest BSP Release available is L4.19.35_1.1.0. You can download the documentation for this BSP on the link below (you may need to login to download this documentation bundle)

https://www.nxp.com/webapp/Download?colCode=L4.19.35_1.1.0_LINUX_DOCS


Inside, you will find the i.MX Yocto Project User's Guide, which has instructions on how to setup Yocto on your host machine to build images for this board.


Regards,