absolute maximum ratings for HDMI signals and clock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

absolute maximum ratings for HDMI signals and clock

1,341件の閲覧回数
diegoperez
Contributor II

Hi,

What is the absolute maximum ratings for HDMI signals and clock? in the imx6 processor:

HDMI_CLKM

HDMI_CLKP

HDMI_D0M
HDMI_D0P

HDMI_D1M

HDMI_D1P

HDMI_D2M
HDMI_D2P

BR

Diego.

ラベル(6)
0 件の賞賛
返信
2 返答(返信)

1,236件の閲覧回数
diegoperez
Contributor II

Hi Igor,

I see in table 59 that the termination voltage of the receiver must be between 3.15 and 3.45. These are the operating conditions, but I would like to know the maximum ratings.

I am studying a problem that causes imx hdmi phy to break, and I suspect it could be due to a transient voltage at power up of receiver board.

BR 

Diego.

0 件の賞賛
返信

1,236件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Diego

it can be found in sect.4.12.7.2 Electrical Characteristics

i.MX 6Dual/6Quad Applications Processors for Consumer Products - Data Sheet

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信