Yocto Project image

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Yocto Project image

2,648件の閲覧回数
srinivasaraopor
Contributor II

Hi,

We have got a freescale IMX6DL processor board. We have followed Yocto training and got the sdcard images which we have deployed to Sd card and power on the board. Now the board is booting to Yocto linux. But we are new this Yocto linux ( We have some knowledge about Ubuntu and Fedora or Redhat).

Where can we get the commands for Yocto. How packages like i2c-tools and others be installed. How update and upgrade (like Debian We will use apt-get update / if it is rpm then yum update)

ラベル(5)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,193件の閲覧回数
art
NXP Employee
NXP Employee

The detailed documentation on the Freescale BSPs (including Yocto) for the i.MX6 series processors is available on the Freescale web site (check the "Supporting Information" section):

http://crm-prod.freescale.net/crm/start.swe?SWECmd=GotoView&SWEView=Detail+Service+Request+List+View...

The same documentation is also available as the part of the BSP packages themselves (check the "Board Support Packages" section):

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREPLAT&fpsp=1&tab=Design_Too...


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,193件の閲覧回数
saurabh206
Senior Contributor III
0 件の賞賛
返信