Yocto Linux defconfig question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Yocto Linux defconfig question

跳至解决方案
2,820 次查看
ottoblom
Contributor III

Hi There,

In the LTIB 4.1.0 BSP release it was very clear which files defined the platform in the arch/mach-imx6 along with a imx6_defconfig file. However, no such luck in the Yocto 1.0.0 BSP. As far as I can tell there is only one defconfig file (imx_v7_defconfig), that confusingly enough defines

CONFIG_SOC_IMX53=y

CONFIG_SOC_IMX6Q=y

CONFIG_SOC_IMX6SL=y

Is this the correct defconfig file for a imx6qsabresd ? And if so, how can one figure that out ? How is the kernel customized if I wanted to build for an imx3 device instead ? I realize the changes to the kernel is made to make it easier to maintain and increase code-reuse and I'm sure it will all make a lot of sense to me later, but not yet.

Thanks in advance and have a great weekend !

/Otto

标签 (3)
标记 (1)
0 项奖励
回复
1 解答
1,748 次查看
ottoblom
Contributor III

Ok, maybe this can help someone else - The Yocto 1.0.0 BSP uses device trees for most of the board-specific items. The top-level dts file for the imx6qsabresd is located at tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/3.10.17-r0/git/arch/arm/boot/dts/imx6q-sabresd.dts. Note that it in turn includes several other files.

Still confusing that the imx_v7_defconfig defines three different IMX SOCs, but maybe there are good reasons for that

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,749 次查看
ottoblom
Contributor III

Ok, maybe this can help someone else - The Yocto 1.0.0 BSP uses device trees for most of the board-specific items. The top-level dts file for the imx6qsabresd is located at tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/3.10.17-r0/git/arch/arm/boot/dts/imx6q-sabresd.dts. Note that it in turn includes several other files.

Still confusing that the imx_v7_defconfig defines three different IMX SOCs, but maybe there are good reasons for that

0 项奖励
回复
1,748 次查看
fabio_estevam
NXP Employee
NXP Employee

imx_v7_defconfig builds all the imx that are armv7: mx51, mx53 and mx6.

In the past we used to have a defconfig per board. Currently we tend to group the defconfigs as much as we can.

0 项奖励
回复