Yocto L4.1.15 is not booting in custom board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Yocto L4.1.15 is not booting in custom board

1,326 Views
jansirani
Contributor III

Hai

we have a custom board same as iMX6SLEVK.

we downloaded Yocto 4.1.15 and compiled fsl-image-gui.

Then by using Mfgtools flashed compiled fsl-image-gui images to sdcard successfully.

But at the booting time it is getting stop at "cpu cpu0: dev_pm_opp_get_opp_count: device OPP not found (-19)" without any errors.

if we use the same sdcard in iMX6SLEVK it is booting properly.

when we compare custom board & iMX6SLEVK logs "cpu cpu0: dev_pm_opp_get_opp_count: device OPP not found (-19)" is coming in both of the logs.

for reference we attached custom board logs and iMX6SLEVK logs .

 

Thanks & Regards,

D.Jansirani

Original Attachment has been moved to: yocto-4.1.15-SLEVK-booting-logs.DAT.zip

Original Attachment has been moved to: yocto-4.1.15-Customboard-booting-logs.DAT.zip

Labels (3)
0 Kudos
Reply
3 Replies

1,150 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jansi

behaviour is correct as "same sdcard" works for iMX6SLEVK but may not work

for new board, so ddr test should be run and new calibration coefficients

should be entered to  uboot *.cfg file, then build new image for custom board

uboot-imx.git - Freescale i.MX u-boot Tree 

https://community.freescale.com/docs/DOC-105652 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,150 Views
jansirani
Contributor III

Thanks for the reply,

But we already tested Marshmallo Demo images in our custom board ,board is booting properly.

But Yocto4.1.15 is not booting.

if it is a ddr problem Marshmallo also should not boot in our custom board .

is this correct or not?

0 Kudos
Reply

1,150 Views
igorpadykov
NXP Employee
NXP Employee

So you did not tested memory with ddr test ?

I do not think that this is right.

In general one can debug it using apnote AN4553 Using Open Source Debugging

Tools for Linux on i.MX Processors

http://www.nxp.com/assets/documents/data/en/application-notes/AN4553.pdf 

0 Kudos
Reply