Toggle timing of the double buffer in i.MX53 IPU

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Toggle timing of the double buffer in i.MX53 IPU

跳至解决方案
1,119 次查看
torus1000
Contributor V

Hi,

I have a question about double buffering feature of i.MX53 IPU.

I know the FSU automatically toggles the DMA_CH_CUR_BUF_# to point on the correct buffer(EBA0 or EBA1) to be used by the channel.

However I would like to toggle it manually by using IPU_CH_BUFx_RDYx register when CH0 transfer done followed by IPU SYNC interrupt(IRQ=11) requested.

In such case when actual toggle will happen? It will switch immediately or wait something?

Can anyone help me? I want to confirm it for the safe screenshot feature.

Thanks.

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,041 次查看
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

I am afraid it is not possible to toggle manually DMA_CH_CUR_BUF as

IPU was not designed for such operation. Also manual register writing would

introduce unpredictable delays, so IPU operates using FSU with automatically

toggling DMA_CH_CUR_BUF.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,042 次查看
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

I am afraid it is not possible to toggle manually DMA_CH_CUR_BUF as

IPU was not designed for such operation. Also manual register writing would

introduce unpredictable delays, so IPU operates using FSU with automatically

toggling DMA_CH_CUR_BUF.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复