Yocto HOB configuration issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Yocto HOB configuration issue

3,231 次查看
sumanranjan
Contributor III

We are using Yocto build system for IMX6 platform. We want to use HOB for package selection or removal. Host system is Ubuntu 12.04.

In the HOB user interface, We selectedimx6qsabresd’ as machine type and ‘core-image-base’ as the base image type. After that if we select 'edit image' and try to add ‘gpu-viv-bin-mx6q’ as it is not part of ‘core-image-base’ then HOB throws below error.


../fsl-community-bsp/build$ hob

Traceback (most recent call last):

  File "/home/vivek/magik2/svn/trunk/i.MX6/linux/yocto/fsl-community-bsp/sources/poky/bitbake/lib/bb/ui/hob.py", line 57, in event_handle_idle_func

    hobHandler.handle_event(event)

  File "/home/vivek/magik2/svn/trunk/i.MX6/linux/yocto/fsl-community-bsp/sources/poky/bitbake/lib/bb/ui/crumbs/hobeventhandler.py", line 253, in handle_event

    self.run_next_command()

  File "/home/vivek/magik2/svn/trunk/i.MX6/linux/yocto/fsl-community-bsp/sources/poky/bitbake/lib/bb/ui/crumbs/hobeventhandler.py", line 180, in run_next_command

    targets[0] += version

TypeError: cannot concatenate 'str' and 'NoneType' objects

^CTraceback (most recent call last):

  File "/home/vivek/magik2/svn/trunk/i.MX6/linux/yocto/fsl-community-bsp/sources/poky/bitbake/bin/bitbake", line 275, in <module>

    ret = main()

  File "/home/vivek/magik2/svn/trunk/i.MX6/linux/yocto/fsl-community-bsp/sources/poky/bitbake/bin/bitbake", line 264, in main

    return server.launchUI(ui_main, server_connection.connection, server_connection.events)

  File "/home/vivek/magik2/svn/trunk/i.MX6/linux/yocto/fsl-community-bsp/sources/poky/bitbake/lib/bb/server/process.py", line 269, in launchUI

    return uifunc(*args)

  File "/home/vivek/magik2/svn/trunk/i.MX6/linux/yocto/fsl-community-bsp/sources/poky/bitbake/lib/bb/ui/hob.py", line 78, in main

    gtk.main()

Any idea what is causing above error ?

~Suman

标签 (2)
标记 (4)
0 项奖励
回复
5 回复数

2,095 次查看
YixingKong
Senior Contributor IV

Suman

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 项奖励
回复

2,095 次查看
tonyzheng
NXP Employee
NXP Employee

Hi, Suman

It is a bug for Yocto on iMX6Q board and i have faced with the same defect also! In my opinion, now there are no better solution for this problem. I hope that Yocto 1.6 for freescale bsp will resolve it. As a workaround, you can use bitbake -c CMD(deploy) instead of  graphic interface as many engineers do. In addition, Yocto 1.6 for iMX6Q should be released in following months.

0 项奖励
回复

2,095 次查看
sumanranjan
Contributor III

Thanks Tao for your reply.

I have started using bitbake commands for yocto build since I could not work around the issue.

0 项奖励
回复

2,095 次查看
YixingKong
Senior Contributor IV

Suman

Is your bitbake command good? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 项奖励
回复

2,095 次查看
ed_martinez
NXP Employee
NXP Employee

Did anybody answer this question? I ran into the same problem and I was about to edit the image and add 'gpu-viv-bin-mx6q' until  saw your results ...

-Ed

0 项奖励
回复