Yocto Desktop reference

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Yocto Desktop reference

3,472 Views
li_hong
Contributor III

Hi Team,

I'm using Yocto project and I use i.MX6 sabre-SD Quad as my platform.

 

I use below Distro and build image with below commands.

  1. DISTRO=fsl-imx-xwayland MACHINE=imx6qsabresd source fsl-setup-release.sh -b build-xwayland-imx6
  2. bitbake fsl-image-qt5-validation-imx

 

I'd bought up successfully, but there is no shortcut icon on the desktop.

Did I miss anything?

How can I solve this problem?

 

Thanks in Advanced!

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

3,301 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Which version of BSP are you using?

0 Kudos
Reply

3,301 Views
li_hong
Contributor III

Hi,Rita:

My repo cmd is “repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-sumo -m
imx-4.14.78-1.0.0_ga.xml”

0 Kudos
Reply

3,301 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

There is no UI, so your action is right. You can playback video to test.

0 Kudos
Reply