Xen compilation problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Xen compilation problem

3,144 Views
dhty2015
Contributor II

hi everone:

Yocto can compile xen module, but I want to compile the updated version of xen, can you give me some Suggestions on how to update the bb file of yocto or how to directly update the latest version of code to compile ~

3 Replies

3,016 Views
igorpadykov
NXP Employee
NXP Employee

Hi yuelin

one can try to follow sect.5.6.11 Building Xen attached Yocto Guide.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,016 Views
dhty2015
Contributor II

The xen version number in the project is 4.11, and my target is 4.12.The version number on the release appears to be version 4.11.So I want to know how to compile imx-xen without yocto, or how to modify the recipe file to upgrade to 4.12.It still doesn't solve my problem

0 Kudos
Reply

3,016 Views
igorpadykov
NXP Employee
NXP Employee

one can look at RELEASE-4.12.0 

imx-xen - i.MX Xen 

0 Kudos
Reply