Xen compilation problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Xen compilation problem

3,138件の閲覧回数
dhty2015
Contributor II

hi everone:

Yocto can compile xen module, but I want to compile the updated version of xen, can you give me some Suggestions on how to update the bb file of yocto or how to directly update the latest version of code to compile ~

3 返答(返信)

3,010件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi yuelin

one can try to follow sect.5.6.11 Building Xen attached Yocto Guide.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,010件の閲覧回数
dhty2015
Contributor II

The xen version number in the project is 4.11, and my target is 4.12.The version number on the release appears to be version 4.11.So I want to know how to compile imx-xen without yocto, or how to modify the recipe file to upgrade to 4.12.It still doesn't solve my problem

0 件の賞賛
返信

3,010件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

one can look at RELEASE-4.12.0 

imx-xen - i.MX Xen 

0 件の賞賛
返信