XML sources for generated C headers and macros

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

XML sources for generated C headers and macros

850 次查看
PetriLaakso1z
Contributor I

Hello Community!

I am studying i.mx23 chip for an open source project which is would be BSD licensed so I cannot use C headers and macros which are available for example in L2.6.31_10.05.02_ER_source/pkgs/imx-bootlets-src-10.05.02. As I read from i.MX233 Reference Manual, Chapter 39, Register Macro Usage, document refers to "chip database" from where these C headers are generated. As far as I know, there are some XML definitions of all registers and some tool is used to convert these XML's to C headers.

Does community have access to these registers definitions? I really would like to use them on my possibly upcoming BSD licensed project.

Yours,

Petri

标记 (2)
0 项奖励
回复
0 回复数