XIP boot feature

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

XIP boot feature

Jump to solution
2,971 Views
o_scherbinin
Contributor III

hello there!
I use MCIMX6SX4_A9.
I want to clarify some points when qspi boot mode implements.
I realaze that even if an uboot image is created with BOOT_FROM qspi and it will be set at right place on a flash device, there would not be XIP boot process while IVT data structure (entry) points to RAM.
(am i right? i suppose in case of xip, the entry have points to flash address)
i would to know how works the engine that swich load proccess to XIP and is it connected with uboot ld file?
Thank you.

1 Solution
2,838 Views
igorpadykov
NXP Employee
NXP Employee

Hi Oleg

yes this understanding is correct and Reference Manual states

pastedImage_1.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
2,839 Views
igorpadykov
NXP Employee
NXP Employee

Hi Oleg

yes this understanding is correct and Reference Manual states

pastedImage_1.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,840 Views
o_scherbinin
Contributor III

Thank you!

0 Kudos
Reply