XIP boot feature

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,001件の閲覧回数
o_scherbinin
Contributor III

hello there!
I use MCIMX6SX4_A9.
I want to clarify some points when qspi boot mode implements.
I realaze that even if an uboot image is created with BOOT_FROM qspi and it will be set at right place on a flash device, there would not be XIP boot process while IVT data structure (entry) points to RAM.
(am i right? i suppose in case of xip, the entry have points to flash address)
i would to know how works the engine that swich load proccess to XIP and is it connected with uboot ld file?
Thank you.

1 解決策
2,868件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Oleg

yes this understanding is correct and Reference Manual states

pastedImage_1.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,869件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Oleg

yes this understanding is correct and Reference Manual states

pastedImage_1.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,870件の閲覧回数
o_scherbinin
Contributor III

Thank you!

0 件の賞賛
返信