XEN Hypervisor DomU Set IP Address

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

XEN Hypervisor DomU Set IP Address

1,601 Views
cbl
Contributor V

Hello,

I am running Yocto image and Android Automotive OS on XEN hypervisor.

Domain-0 Yocto image. DomU is Android Automotive OS.

After creating DomU I want to give IP to DomU. However, I want to run "xl console DomU" command and do it via Domain-0, not from Android Terminal.

But I don't know how to do it. Can you help with this?

What linux command or what XEN configuration do I need to set the IP of DomU@ from Domain-0?

Best regards,

0 Kudos
Reply
2 Replies

1,590 Views
cbl
Contributor V

Hello,

I assigned the ip to DomU using tmux from the terminal of Domain-0 and this is how I solved the problem.

Best regards,

Efecan

0 Kudos
Reply

1,587 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Good!